Post Go back to editing

Download initCal results for fastlock performan

Category: Hardware
Product Number: ADRV9009

I am controlling the ADRV9009 from an FPGA, while the hopRfPll option allows retuning, I was wondering if it was possible to initialise all frequencies, download the results from their initCals, and then reprogram them at a later time (akin to the process explained in AN-1353)?

I am tuning between 4 frequencies which are known at the chip initialisation time. However due to the setup of the rest of the custom RF board having the 2deep FIFO present in the RfHopPll is complicates the FPGA design, and leads to needing to issue the hopRfPll command twice in close succession.