Post Go back to editing

Register Map document for ADRV9008-1

Category: Datasheet/Specs

Hi,


I'm integrating the ADRV9008-1 with a Xilinx KU115 FPGA via custom RTL for SPI/ JESD communication, without using a soft processor like MicroBlaze due to high resource consumption concerns. The datasheets and UG-1295 manual don't include a direct register map

I've checked the no-OS API source on GitHub (talise_reg_addr_macros.h), which seems to contain register address macros used for talSpiWrite/talSpiRead. However, for bare-metal RTL implementation:

  • Is there a complete, official SPI/JESD register map (addresses, bit fields, read/write sequences) available?
  • Are there any guidelines or examples for direct register access without the full API?
  • Or can you suggest any other methods to implement the same.
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.