I'm using ADRV9008-2 at 491.52 MSPS for TX and ORX.
I'm working on ZCU102 + ADRV9008-2 W/PCBZ boards, with no-OS firmware.
This is workink fine if I set the RF frequency to 280MHz and above.
If I set the RF frequency at 270MHz I get this consle output:
Zynq MP First Stage Boot Loader
Release 2023.2 Jun 18 2025 - 07:00:25
PMU-FW is not running, certain applications may not be supported.
Hello
tx_clkgen: MMCM-PLL locked (245760000 Hz)
rx_os_clkgen: MMCM-PLL locked (245760000 Hz)
tx_adxcvr: OK (9830400 kHz)
rx_os_adxcvr: OK (9830400 kHz)
talise: Device Revision 192, Firmware 6.2.1, API 3.6.2.4294967297
ERROR: 294: TALISE_waitArmCmdStatus() failed due to thrown ARM error. Is device in correct state for calling command?
ERROR: 131086: Talise init calibration error encountered
error: TALISE_waitInitCals() failed
Bye
This is strange because I think that in my case it must be possible to have a RF frequency down to 245.76MHz.
Actually if I try to set an RF frequency below this value I get a message tha the RF frequency is too low.
I use this talise_config.c file:
/**
* \file talise_config.c
* \brief Contains Talise configuration settings for the Talise API
*
* Copyright 2015-2017 Analog Devices Inc.
* Released under the AD9378-AD9379 API license, for more information see the "LICENSE.txt" file in this zip file.
*
* The top level structure taliseDevice_t talDevice uses keyword
* extern to allow the application layer main() to have visibility
* to these settings.
*
* This file may not be fully complete for the end user application and
* may need to updated for AGC, GPIO, and DAC full scale settings.
* To create a full initialisation routine, the user should also refer to the
* Iron Python initialisation routine generated by the GUI, and also the Talise User Guide.
*
*/
#include "talise_types.h"
#include "talise_error.h"
#include "talise_agc.h"
#ifdef ADI_ZYNQ_PLATFORM
#include "zynq_platform.h"
#endif
#include "../WorkingProfile/talise_config.h"
int16_t txFirCoefs[20] = {-3, 9, -28, 69, -131, 246, -507, 1182, -2648, 19449, -2648, 1182, -507, 246, -131, 69, -28, 9, -3, 0};
int16_t obsrxFirCoefs[24] = {61, -9, 8, -6, -2, 12, -55, 91, -192, 460, -1719, 19205, -1719, 460, -192, 91, -55, 12, -2, -6, 8, -9, 61, 0};
#ifdef ADI_ZYNQ_PLATFORM /** < Insert Customer Platform HAL State Container here>*/
/*
* Platform Layer SPI settings - this structure is specific to ADI's platform layer code.
* User should replace with their own structure or settings for their hardware
*/
zynqSpiSettings_t spiDev1 =
{
.chipSelectIndex = 1,
.writeBitPolarity = 0,
.longInstructionWord = 1,
.CPHA = 0,
.CPOL = 0,
.mode = 0,
.spiClkFreq_Hz = 25000000
};
/*
* Platform Layer settings - this structure is specific to ADI's platform layer code.
* User should replace with their own structure or settings for their hardware
* The structure is held in taliseDevice_t below as a void pointer, allowing
* the customer to pass any information for their specific hardware down to the
* hardware layer code.
*/
zynqAdiDev_t talDevHalInfo =
{
.devIndex = 1,
.spiSettings = &spiDev1,
.spiErrCode = 0,
.timerErrCode = 0,
.gpioErrCode = 0,
.logLevel = ADIHAL_LOG_ALL
};
#endif
/**
* TalDevice a structure used by the Talise API to hold the platform hardware
* structure information, as well as an internal Talise API state container
* (devStateInfo) of runtime information used by the API.
**/
taliseDevice_t talDevice =
{
#ifdef ADI_ZYNQ_PLATFORM
/* Void pointer of users platform HAL settings to pass to HAL layer calls
* Talise API does not use the devHalInfo member */
.devHalInfo = &talDevHalInfo,
#else
.devHalInfo = NULL, /*/** < Insert Customer Platform HAL State Container here>*/
#endif
/* devStateInfo is maintained internal to the Talise API, just create the memory */
.devStateInfo = {0}
};
taliseInit_t talInit =
{
/* SPI settings */
.spiSettings =
{
.MSBFirst = 1, /* 1 = MSBFirst, 0 = LSBFirst */
.enSpiStreaming = 0, /* Not implemented in ADIs platform layer. SW feature to improve SPI throughput */
.autoIncAddrUp = 1, /* Not implemented in ADIs platform layer. For SPI Streaming, set address increment direction. 1= next addr = addr+1, 0:addr=addr-1 */
.fourWireMode = 1, /* 1: Use 4-wire SPI, 0: 3-wire SPI (SDIO pin is bidirectional). NOTE: ADI's FPGA platform always uses 4-wire mode */
.cmosPadDrvStrength = TAL_CMOSPAD_DRV_2X /* Drive strength of CMOS pads when used as outputs (SDIO, SDO, GP_INTERRUPT, GPIO 1, GPIO 0) */
},
/* Tx settings */
.tx =
{
.txProfile =
{
.dacDiv = 1, /* The divider used to generate the DAC clock */
.txFir =
{
.gain_dB = 0, /* filter gain */
.numFirCoefs = 20, /* number of coefficients in the FIR filter */
.coefs = &txFirCoefs[0]
},
.txFirInterpolation = 1, /* The Tx digital FIR filter interpolation (1,2,4) */
.thb1Interpolation = 2, /* Tx Halfband1 filter interpolation (1,2) */
.thb2Interpolation = 2, /* Tx Halfband2 filter interpolation (1,2)*/
.thb3Interpolation = 1, /* Tx Halfband3 filter interpolation (1,2)*/
.txInt5Interpolation = 1, /* Tx Int5 filter interpolation (1,5) */
.txInputRate_kHz = 491520, /* Primary Signal BW */
.primarySigBandwidth_Hz = 200000000, /* The Rx RF passband bandwidth for the profile */
.rfBandwidth_Hz = 450000000, /* The Tx RF passband bandwidth for the profile */
.txDac3dBCorner_kHz = 450000, /* The DAC filter 3dB corner in kHz */
.txBbf3dBCorner_kHz = 225000, /* The BBF 3dB corner in kHz */
.loopBackAdcProfile = {150, 178, 181, 90, 1280, 1338, 1699, 493, 1386, 162, 934, 4, 48, 46, 35, 201, 0, 0, 0, 0, 50, 0, 0, 6, 24, 0, 0, 6, 24, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 15, 905}
},
.deframerSel = TAL_DEFRAMER_A, /* Talise JESD204b deframer config for the Tx data path */
.txChannels = TAL_TX1TX2, /* The desired Tx channels to enable during initialization */
.txAttenStepSize = TAL_TXATTEN_0P05_DB, /* Tx Attenuation step size */
.tx1Atten_mdB = 0, /* Initial Tx1 Attenuation */
.tx2Atten_mdB = 0, /* Initial Tx2 Attenuation */
.disTxDataIfPllUnlock = TAL_TXDIS_TX_RAMP_DOWN_TO_ZERO /* Options to disable the transmit data when the RFPLL unlocks. */
},
/* ObsRx settings */
.obsRx =
{
.orxProfile =
{
.rxFir =
{
.gain_dB = -6, /* filter gain */
.numFirCoefs = 24, /* number of coefficients in the FIR filter */
.coefs = &obsrxFirCoefs[0]
},
.rxFirDecimation = 1, /* Rx FIR decimation (1,2,4) */
.rxDec5Decimation = 4, /* Decimation of Dec5 or Dec4 filter (5,4) */
.rhb1Decimation = 1, /* RX Half band 1 decimation (1 or 2) */
.orxOutputRate_kHz = 491520, /* Rx IQ data rate in kHz */
.rfBandwidth_Hz = 450000000, /* The Rx RF passband bandwidth for the profile */
.rxBbf3dBCorner_kHz = 225000, /* Rx BBF 3dB corner in kHz */
.orxLowPassAdcProfile = {155, 163, 181, 90, 1280, 1254, 1572, 340, 1431, 142, 973, 8, 48, 47, 36, 205, 0, 0, 0, 0, 51, 0, 0, 6, 24, 0, 0, 6, 24, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 15, 905},
.orxBandPassAdcProfile = {124, 131, 154, 90, 1280, 2779, 1986, 0, 1037, 839, 988, 109, 11, 15, 28, 179, 0, 0, 0, 0, 45, 0, 0, 0, 24, 0, 0, 0, 24, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 15, 905},
.orxDdcMode = TAL_ORXDDC_DISABLED, /* ORx DDC mode */
.orxMergeFilter = {-167, 419, -208, -498, 968, -320, -1273, 2154, -402, -4155, 9170, 21413}
},
.orxGainCtrl =
{
.gainMode = TAL_MGC,
.orx1GainIndex = 255,
.orx2GainIndex = 255,
.orx1MaxGainIndex = 255,
.orx1MinGainIndex = 195,
.orx2MaxGainIndex = 255,
.orx2MinGainIndex = 195
},
.framerSel = TAL_FRAMER_B, /* ObsRx JESD204b framer configuration */
.obsRxChannelsEnable = TAL_ORX1, /* The desired ObsRx Channels to enable during initialization */
.obsRxLoSource = TAL_OBSLO_RF_PLL /* The ORx mixers can use the TX_PLL */
},
/* Digital Clock Settings */
.clocks =
{
.deviceClock_kHz = 245760, /* CLKPLL and device reference clock frequency in kHz */
.clkPllVcoFreq_kHz = 9830400, /* CLKPLL VCO frequency in kHz */
.clkPllHsDiv = TAL_HSDIV_2P5, /* CLKPLL high speed clock divider */
.rfPllUseExternalLo = 0, /* 1= Use external LO for RF PLL, 0 = use internal LO generation for RF PLL */
.rfPllPhaseSyncMode = TAL_RFPLLMCS_INIT_AND_CONTTRACK /* RFPLL MCS (Phase sync) mode */
},
/* JESD204B settings */
.jesd204Settings =
{
/* Framer B settings */
.framerB =
{
.bankId = 0, /* JESD204B Configuration Bank ID -extension to Device ID (Valid 0..15) */
.deviceId = 0, /* JESD204B Configuration Device ID - link identification number. (Valid 0..255) */
.lane0Id = 0, /* JESD204B Configuration starting Lane ID. If more than one lane used, each lane will increment from the Lane0 ID. (Valid 0..31) */
.M = 2, /* number of ADCs (0, 2, or 4) - 2 ADCs per receive chain */
.K = 32, /* number of frames in a multiframe (default=32), F*K must be a multiple of 4. (F=2*M/numberOfLanes) */
.F = 2, /* F (number of bytes per frame) */
.Np = 16, /* Np (converter sample resolution) */
.scramble = 1, /* scrambling off if framerScramble= 0, if framerScramble>0 scramble is enabled. */
.externalSysref = 1, /* 0=use internal SYSREF, 1= use external SYSREF */
.serializerLanesEnabled = 0x0C, /* serializerLanesEnabled - bit per lane, [0] = Lane0 enabled, [1] = Lane1 enabled */
.serializerLaneCrossbar = 0xE4, /* serializerLaneCrossbar */
.lmfcOffset = 31, /* lmfcOffset - LMFC offset value for deterministic latency setting */
.newSysrefOnRelink = 0, /* newSysrefOnRelink */
.syncbInSelect = 1, /* syncbInSelect; */
.overSample = 0, /* 1=overSample, 0=bitRepeat */
.syncbInLvdsMode = 1,
.syncbInLvdsPnInvert = 0,
.enableManualLaneXbar = 0 /* 0=auto, 1=manual */
},
/* Framer A settings */
.framerA =
{
.bankId = 0, /* JESD204B Configuration Bank ID -extension to Device ID (Valid 0..15) */
.deviceId = 0, /* JESD204B Configuration Device ID - link identification number. (Valid 0..255) */
.lane0Id = 0, /* JESD204B Configuration starting Lane ID. If more than one lane used, each lane will increment from the Lane0 ID. (Valid 0..31) */
.M = 2, /* number of ADCs (0, 2, or 4) - 2 ADCs per receive chain */
.K = 32, /* number of frames in a multiframe (default=32), F*K must be a multiple of 4. (F=2*M/numberOfLanes) */
.F = 0, /* F (number of bytes per frame) */
.Np = 16, /* Np (converter sample resolution) */
.scramble = 1, /* scrambling off if framerScramble= 0, if framerScramble>0 scramble is enabled. */
.externalSysref = 1, /* 0=use internal SYSREF, 1= use external SYSREF */
.serializerLanesEnabled = 0x03, /* serializerLanesEnabled - bit per lane, [0] = Lane0 enabled, [1] = Lane1 enabled */
.serializerLaneCrossbar = 0xE4, /* serializerLaneCrossbar */
.lmfcOffset = 31, /* lmfcOffset - LMFC offset value for deterministic latency setting */
.newSysrefOnRelink = 0, /* newSysrefOnRelink */
.syncbInSelect = 1, /* syncbInSelect; */
.overSample = 0, /* 1=overSample, 0=bitRepeat */
.syncbInLvdsMode = 1,
.syncbInLvdsPnInvert = 0,
.enableManualLaneXbar = 0 /* 0=auto, 1=manual */
},
/* Deframer A settings */
.deframerA =
{
.bankId = 0, /* bankId extension to Device ID (Valid 0..15) */
.deviceId = 0, /* deviceId link identification number. (Valid 0..255) */
.lane0Id = 0, /* lane0Id Lane0 ID. (Valid 0..31) */
.M = 4, /* M number of DACss (0, 2, or 4) - 2 DACs per transmit chain */
.K = 32, /* K #frames in a multiframe (default=32), F*K=multiple of 4. (F=2*M/numberOfLanes) */
.scramble = 1, /* scramble scrambling off if scramble= 0 */
.externalSysref = 1, /* externalSysref 0= use internal SYSREF, 1= external SYSREF */
.deserializerLanesEnabled = 0x0F, /* deserializerLanesEnabled bit per lane, [0] = Lane0 enabled */
.deserializerLaneCrossbar = 0xE4, /* deserializerLaneCrossbar */
.lmfcOffset = 17, /* lmfcOffset LMFC offset value to adjust deterministic latency */
.newSysrefOnRelink = 0, /* newSysrefOnRelink */
.syncbOutSelect = 0, /* SYNCBOUT0/1 select */
.Np = 16, /* Np (converter sample resolution) */
.syncbOutLvdsMode = 1,
.syncbOutLvdsPnInvert = 0,
.syncbOutCmosSlewRate = 0,
.syncbOutCmosDriveLevel = 0,
.enableManualLaneXbar = 0 /* 0=auto, 1=manual */
},
/* Deframer B settings */
.deframerB =
{
.bankId = 0, /* bankId extension to Device ID (Valid 0..15) */
.deviceId = 0, /* deviceId link identification number. (Valid 0..255) */
.lane0Id = 0, /* lane0Id Lane0 ID. (Valid 0..31) */
.M = 0, /* M number of DACss (0, 2, or 4) - 2 DACs per transmit chain */
.K = 32, /* K #frames in a multiframe (default=32), F*K=multiple of 4. (F=2*M/numberOfLanes) */
.scramble = 1, /* scramble scrambling off if scramble= 0 */
.externalSysref = 1, /* externalSysref 0= use internal SYSREF, 1= external SYSREF */
.deserializerLanesEnabled = 0x00, /* deserializerLanesEnabled bit per lane, [0] = Lane0 enabled */
.deserializerLaneCrossbar = 0xE4, /* deserializerLaneCrossbar */
.lmfcOffset = 0, /* lmfcOffset LMFC offset value to adjust deterministic latency */
.newSysrefOnRelink = 0, /* newSysrefOnRelink */
.syncbOutSelect = 1, /* SYNCBOUT0/1 select */
.Np = 16, /* Np (converter sample resolution) */
.syncbOutLvdsMode = 1,
.syncbOutLvdsPnInvert = 0,
.syncbOutCmosSlewRate = 0,
.syncbOutCmosDriveLevel = 0,
.enableManualLaneXbar = 0 /* 0=auto, 1=manual */
},
.serAmplitude = 15, /* Serializer amplitude setting. Default = 15. Range is 0..15 */
.serPreEmphasis = 1, /* Serializer pre-emphasis setting. Default = 1 Range is 0..4 */
.serInvertLanePolarity = 0, /* Serializer Lane PN inversion select. Default = 0. Where, bit[0] = 1 will invert lane [0], bit[1] = 1 will invert lane 1, etc. */
.desInvertLanePolarity = 0, /* Deserializer Lane PN inversion select. bit[0] = 1 Invert PN of Lane 0, bit[1] = Invert PN of Lane 1, etc */
.desEqSetting = 1, /* Deserializer Equalizer setting. Applied to all deserializer lanes. Range is 0..4 */
.sysrefLvdsMode = 1, /* Use LVDS inputs on Talise for SYSREF */
.sysrefLvdsPnInvert = 0 /*0= Do not PN invert SYSREF */
}
};
//Only needs to be called if user wants to setup AGC parameters
static taliseAgcCfg_t rxAgcCtrl =
{
4,
255,
195,
255,
195,
30720, /* AGC gain update time in us (125us-250us - based on IQ data rate - set for 125us @ 245.76 Mhz) */
10,
10,
16,
0,
1,
0,
0,
0,
1,
31,
246,
4,
1, /*!<1- bit field to enable the multiple time constants in AGC loop for fast attack and fast recovery to max gain. */
/* agcPower */
{
1, /*!<1-bit field, enables the Rx power measurement block. */
1, /*!<1-bit field, allows using Rx PFIR for power measurement. */
0, /*!<1-bit field, allows to use the output of the second digital offset block in the Rx datapath for power measurement. */
9, /*!<AGC power measurement detect lower 0 threshold. Default = -12dBFS == 5, 7-bit register value where max = 0x7F, min = 0x00 */
2, /*!<AGC power measurement detect lower 1 threshold. Default = (offset) 4dB == 0, 4-bit register value where max = 0xF, min = 0x00 */
4, /*!<AGC power measurement detect lower 0 recovery gain step. Default = 2dB - based on gain table step size, 5-bit register value where max = 0x1F, min = 0x00 */
4, /*!<AGC power measurement detect lower 1 recovery gain step. Default = 4dB - based on gain table step size, 5-bit register value where max = 0x1F, min = 0x00 */
5, /*!< power measurement duration used by the decimated power block. Default = 0x05, 5-bit register value where max = 0x1F, min = 0x00 */
5, /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
1, /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
5, /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
1, /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
2, /*!<Default value should be 2*/
0,
0
},
/* agcPeak */
{
205, /*!<1st update interval for the multiple time constant in AGC loop mode, Default:205. */
2, /*!<sets the 2nd update interval for the multiple time constant in AGC loop mode. Calculated as a multiple of agcUnderRangeLowInterval , Default: 4 */
4, /*!<sets the 3rd update interval for the multiple time constant in AGC loop mode. Calculated as a multiple of agcUnderRangeMidInterval and agcUnderRangeLowInterval, Default: 4 */
39, /*!<AGC APD high threshold. Default=0x1F, 6-bit register value where max=0x3F, min =0x00 */
49, /*!<AGC APD peak detect high threshold. default = 0x1F, 6-bit register value where max = 0x3F, min = 0x00. Set to 3dB below apdHighThresh */
23, /*!<AGC APD peak detect low threshold. default = 3dB below high threshold, 6-bit register value where max =0x3F, min = 0x00 */
19, /*!<AGC APD peak detect low threshold. default = 3dB below high threshold, 6-bit register value where max = 0x3F, min = 0x00 . Set to 3dB below apdLowThresh */
6, /*!<AGC APD peak detect upper threshold count. Default = 0x06 8-bit register value where max = 0xFF, min = 0x20 */
3, /*!<AGC APD peak detect lower threshold count. Default = 0x03, 8-bit register value where max = 0xFF, min = 0x00 */
4, /*!<AGC APD peak detect attack gain step. Default = 2dB step - based on gain table step size, 5-bit register value, where max = 0x1F, min = 0x00 */
2, /*!<AGC APD gain index step size. Recommended to be same as hb2GainStepRecovery. Default = 0x00, 5-bit register value where max = 0x1F, min = 0x00 */
1, /*!<1-bit field, enables or disables the HB2 overload detector. */
1, /*!<3-bit field. Sets the window of clock cycles (at the HB2 output rate) to meet the overload count. */
1, /*!<4-bit field. Sets the number of actual overloads required to trigger the overload signal. */
181, /*!<AGC decimator output high threshold. Default = 0xB5, 8-bit register value where max = 0xFF, min = 0x00 */
45, /*!<AGC decimator output low threshold. Default = 0x80, 8-bit register value where max = 0xFF, min = 0x00 */
90, /*!<AGC decimator output low threshold. Default = 0x80, 8-bit register value where max = 0xFF, min = 0x00 */
128, /*!<AGC decimator output low threshold. Default = 0x80, 8-bit register value where max = 0xFF, min = 0x00 */
6, /*!<AGC HB2 output upper threshold count. Default = 0x06, 8-bit register value where max = 0xFF, min = 0x20 */
3, /*!<AGC HB2 output lower threshold count. Default = 0x03, 8-bit register value where max = 0xFF, min = 0x00 */
2, /*!<AGC decimator gain index step size. Default = 0x00, 5-bit register value where max = 0x1F, min = 0x00 */
4, /*!<AGC HB2 gain index step size, when the HB2 Low Overrange interval 0 triggers a programmable number of times. Default = 0x08, 5-bit register value where max = 0x1F, min = 0x00 */
8, /*!<AGC HB2 gain index step size, when the HB2 Low Overrange interval 1 triggers a programmable number of times. Default = 0x04, 5-bit register value where max = 0x1F, min = 0x00 */
4, /*!<AGC decimator output attack gain step. Default = 2dB step - based on gain table step size, 5-bit register value, where max = 0x1F, min = 0x00 */
1,
0,
0
}
};
Any suggestion?
Thasnk you
Maurizio Sonzogni