Post Go back to editing

Phase synchronization not working with recent API

Category: Software
Product Number: ADRV9009
Software Version: API 3.6.2.1

We have custom boards with ADRV9009. We need to have a known phase between the reference clock and the RF output. We have achieved that following

https://ez.analog.com/rf/wide-band-rf-transceivers/tes-gui-software-support-adrv9009-adrv9008-1-adrv9008-2/f/q-a/122649/talise_enablemultichiprflophasesync-and-talise_enablemultichipsync-which-order

In other words it is working with following revisions:

Talise: Device Revision 192, Firmware 6.0.2, API 3.6.0.5

But it is not working with a newer version:

Talise: Device Revision 192, Firmware 6.2.1, API 3.6.2.1

Why is it so? What are the differences between the versions?

Side remark: TALISE_enableMultichipRfLOPhaseSync is still not mentioned at all in UG-1295, as far as I know.

Thread Notes

  • It should be working with the latest version as well. The UG-1295 doesn't have these details mentioned, you can see the below API definition from source file package.

    /*From source file package*/
    * \brief Sets up the chip for multichip LOs Phase synchronization
    LOs on multiple chips can be phase synchronized to support active antenna system and beam forming applications.

    This function should be run after all transceivers have finished the TALISE_setRfPllFrequency(), and before TALISE_runInitCals().
    * When the enableDigTestClk parameter = 1, this function will reset the MCS state machine in the Talise device and switch the ARM to run on device clock scaled instead of HSDIGCLK
    * When the enableDigTestClk parameter = 0, this function will enable Mcs Digital Clocks Sync and JESD204 sysref,
    * switch the ARM back the HSDIGCLK.
    * Typical sequence:
    * 1) Initialize all Talise devices in system using TALISE_initialize(),load the ARM and stream processor
    * 2) Set the RF PLL frequency with TALISE_setRfPllFrequency
    * 3) Run TALISE_enableMultichipRfLOPhaseSync with enableDigTestClk = 1 before TALISE_runInitCals()
    * 4) Send at least 4 SYSREF pulses
    * 5) Run TALISE_enableMultichipRfLOPhaseSync with enableDigTestClk = 0
    * 6) Send at least 4 SYSREF pulses
    * 7) Continue with init sequence ...Run initCals, bring up JESD204, etc
    *
    * \pre This function is called after the device has been initialized, ARM is loaded and PLL lock status has
    * been verified

    * \param device is a pointer to the device settings structure
    * \param enableDigTestClk =1 will enable/reset the MCS state machine and switch between device clock scaled and
    * HSDIGCLK

    uint32_t TALISE_enableMultichipRfLOPhaseSync(taliseDevice_t *device, uint8_t enableDigTestClk

    Do you see any error while enabling phase synchronization , can you please share us the error log and observations in detail.

    Can you please share us the test setup diagram as well.