Post Go back to editing

SD image

Thread Summary

The user encountered issues with eth0 after updating ZC706 platform files using the ADRV-9009 TES GUI. The problem was resolved by re-flashing the SD card with the AD9371 image file. The final answer suggests downloading the AD9371 image and building the SD card from the ADRV9009-SD card folder, available at the provided Analog Devices link.
AI Generated Content
Category: Hardware
Product Number: ADRV9009

Hi, there :

I follow the suggestion to download AD9371 image file and update the platform files using ADRV-9009 TES GUI into ZC706 board.

After the platform files are updated, ZC706 board reboot but something wrong with eth0. 

During ZC706 board reboot, the console show the below message. (eth0 is lost)

xemacps e000b000.eth: eth0: no PHY foundterminated with status 5
xemacps e000b000.eth: XEMACPS mii bus mii_probe fail.

I reflash SD card with AD9371 image file and then ZC706 board can boot up normally. (eth0 exist)

I tried this procedure several times and it always happened.

Is there any way to fix this problem? or ADI has a image file for ADRV-9008/9009?

Although ADI has a updated file - "ADRV9009-SDCARD.zip" on the web site, but it's not a image file. (Can't flash into SD card)

Please help & thanks.

Yao-Hua

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.