ADRV9009
Recommended for New Designs
The ADRV9009 is a highly integrated, radio frequency (RF), agile transceiver offering dual transmitters and receivers, integrated synthesizers, and digital...
Datasheet
ADRV9009 on Analog.com
HI Team,
I am working ZCU102 interface with ADRV9009,we are using Frequency hopping GPIO mode function ,when we are changing frequency from one to another we observe that we are not getting the LO that we have tuned. When we call the hopping function in a continuous loop we are able to see that the LO is being set. When we call it once or twice it is not working. Could you please guide to resolve this issue?
__CommunityServer__Service__ - Moved from TES GUI & Software support ADRV9009/ADRV9008-1/ADRV9008-2 to Design Support ADRV9008-1/ADRV9008-2/ADRV9009. Post date updated from Wednesday, July 10, 2024 5:02 AM UTC to Thursday, January 22, 2026 7:55 PM UTC to reflect the move.
Please confirm whether you are using the ZCU102 board with the ADRV900x evaluation board. Are you using the GPIO mode to control the frequency change? If you are using the GPIO mode and need to assign frequency hopping GPIO during initialization time, the next hopping frequency must be set via an API command. Please refer to the RF PLL FREQUENCY HOPPING section in the ADRV900x reference manual.
Please confirm whether you are using the ZCU102 board with the ADRV900x evaluation board. Are you using the GPIO mode to control the frequency change? If you are using the GPIO mode and need to assign frequency hopping GPIO during initialization time, the next hopping frequency must be set via an API command. Please refer to the RF PLL FREQUENCY HOPPING section in the ADRV900x reference manual.