Post Go back to editing

Tx Interface rate to support 40 MHz Sampling Bandwidth?

Category: Hardware
Product Number: ADRV9009

Greetings ADI,

I am working to sample RF within a bandwidth of 46.08 MHz, and I was planning to transmit the IQ data at double this rate. However the provided interface rates in Table 7, page 100 of the documentation only depict four examples. How should I proceed with establishing a custom transmitting frequency compatible with our specifications? If this capability is enabled within the user design files, how should I go about modifying them?

Many thanks.

Thread Notes