HMC7044
Recommended for New Designs
The HMC7044 is a high performance, dual-loop, integer-N jitter attenuator capable of performing reference selection and generation of ultralow phase noise...
HMC7044 on Analog.com
ADRV9009
Recommended for New Designs
The ADRV9009 is a highly integrated, radio frequency (RF), agile transceiver offering dual transmitters and receivers, integrated synthesizers, and digital...
Datasheet
ADRV9009 on Analog.com
Hi, we have a high frequency application requiring tight frequency stability. To minimize drift:
Your assistance is highly appreciated.
Dorant - Moved from RF and Microwave to Design Support ADRV9008-1/ADRV9008-2/ADRV9009. Post date updated from Friday, January 19, 2024 11:02 PM UTC to Monday, January 22, 2024 1:37 PM UTC to reflect the move.
1. You can't replace the VCXO with an OCXO, charge pump out is coming from HMC7044 and controlling the frequency of the VCXO, another thing is note is the VCXO part used in the design is an ultra-low-noise phase oscillator, and not sure what kind of part are you planning to use.
2. For HMC7044-related questions please open a new post with specific questions in the below forum.
3. What is your requirement for frequency drift? were you able to measure the drift with the existing design?
4. PLL1 accepts up to four references and one of them is getting from TCXO, please refer to the HMC7044 datasheet PLL1 Reference inputs section for more details.
1. You can't replace the VCXO with an OCXO, charge pump out is coming from HMC7044 and controlling the frequency of the VCXO, another thing is note is the VCXO part used in the design is an ultra-low-noise phase oscillator, and not sure what kind of part are you planning to use.
2. For HMC7044-related questions please open a new post with specific questions in the below forum.
3. What is your requirement for frequency drift? were you able to measure the drift with the existing design?
4. PLL1 accepts up to four references and one of them is getting from TCXO, please refer to the HMC7044 datasheet PLL1 Reference inputs section for more details.
We looked at the HMC7044 datasheet again and the PLL1 General Description makes clear that the function of PLL1 is to lock a clean VCXO to the average frequency of one of the input references and feed it to PLL2 to generate a high quality clock for local use.
We would have preferred a 0.5 ppm TCXO but we'll start with what comes with the SoM and use an external reference or fixed offset as required at operating temperature