Post Go back to editing

Reduce the passband of RX path to minimum.(according with data sheet the RX BW is 10MHz)

Thread Summary

The user wants to configure the ADRV9009 (Talise) to reduce the RX path passband to 3 MHz from the current 50 MHz, with a sample clock of 122.88 MSample/sec. The final answer suggests using the Talise configuration wizard to generate the required profiles and program the chip through the TES GUI. The data sheet indicates the minimum RX BW is 10 MHz, which may limit further reduction.
AI Generated Content
Category: Hardware
Product Number: adrv9009

Hi,

in my design I use the ADRV9009.(Talise) I want to configure the Talise TX path and RX path to work with the signal BW passband (primary BW) for RX and TX =3MHz. My The sample clock for TX and RX is 122.88MSample/sec.

I works with TES SW. I generate profile with 1228MSample/sec. I receive the passband ~50MHz. I want to reduce the passband of RX path to minimum.(according with data sheet the RX BW is 10MHz). Is it possible?

If yes, please advise how?

Thanks

Haim

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.