KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADRV9009
Recommended for New Designs
The ADRV9009 is a highly integrated, radio frequency (RF), agile transceiver offering dual transmitters and receivers, integrated synthesizers, and digital...
Datasheet
ADRV9009 on Analog.com
Hi
Setup:
I am working on custom board based on ADRV9009 and xczu9eg-ffvb1156-2 Xilinx FPGA. I am using no-os based setup.
I am using the profile generate by the TES software with Rx(both) 245.76 MHz, Tx(both) 245.76 MHz, and ORx(both) 245.76MHz.
It is mentioned in the ADRV9009 Datasheet that its has inherent antialiasing features.

Also in the ADRV9009 TES software, the following response is generated in the Rx Summary tab. This composite response shows that the harmonics will be attenuated by over120db.

There are settings in the talise_config.c file for the adc filter (rxAdcProfile). I believe that they contain the setting for this above mentioned behaviour.

Issue:
I see the following issue in the received Rx spectrum:
Questions:
Thanks
Bill
Is there any update on this issue?
Is there any update on this issue?
The third order harmonics and its levels at 80-90dBC are expected as per datasheet specs. There is no way to reduce the levels further, you need to use external filters in order to completely eliminate them.
Test the harmonics at the below conditions with a reduced tone power level of -20dBm .

as per the image:
The composite response shows that the output will be around suppressed by roughly 150dbm. I am assuming the response of this filer. Even when I am giving the input power of -20dBm, the 3rd harmonic peak is 40dbm below the original peak. But as per your argument:
The third order harmonics and its levels at 80-90dBC are expected as per datasheet specs. There is no way to reduce the levels further, you need to use external filters in order to completely eliminate them.
the 3rd harmonic peak should be 80dbm below. So I am again back in the same boat, what should I must do to reduce the 3rd harmonic peak?
Thanks
what is the level are you getting for the 3rd harmonic, you need to use external filtering to suppress them.
For the 3rd harmonic I am getting only 3-4 dB down. Yes external filter is the only way I could opt. But as per the diagram anti aliasing should work.