Hi Team,
I am using FMCOMMS8_ZCU102 setup with a 200MHz bandwidth receiver, sampling at 245.76Msps. The ADRV9009 LO was tuned to 2590MHz and I am providing input of 2451MHz with the help of signal generator at receiver side. Now I exported the CSV of receiver data and plotted the FFT then I am observing the output peak at 2697MHz (fm+fs) which was out of band frequency for my current LO but it acts as in band frequency when I tuned LO to 2690MHz. In general, I observed that, on feeding an input frequency that is in out-of-band-region, the receiver places the signal at (fm + fs), which fall in-band for a different LO-tuning. Why does this happen and are there any ways to solve this issue, as in my application this is not acceptable: I keep hopping between different LOs consecutively.
Thanks & Regards
Goli Ganesh