Post Go back to editing

ADRV9009 Metalic Enclosure

Category: Hardware
Product Number: ADRV9009

May we put a metalic enclosure above the ADRV9009 ?

The distance (in Z direction) between the ADRV9009 case and the metalic enclosure is 1mm.

The ADRV9009 performance should remain the same ?

Thanks

Top Replies

    •  Analog Employees 
    in reply to Dorant +1 verified
    The ADRV9009 performance should remain the same ?

    It should not disturb performance . 

    Why do you want to design a shield which has only 1mm gap?

Parents Reply Children