Hi,
ADRV9008-1/2, user guide says that it can achieve frequency hopping within 70us...This 70 us calibration time includes QEC and DC offset calibration or we have to allot calibration time to do these DC offset calibration, TX/RX quadrature calibration separately if frequency changes more than 100 MHz...
If not so, can we use stored calibration coefficients of DC offset calibration and quadrature calibration on-the-fly if application changes more than 100 MHz from the last calibrated frequency like possibility in AD9361 to reduce calibration time and retain RF performance in hopping mode.
regards,
lakshmi