I am using the ADRV9009 evaluation board. I would like to reconfigure the board to use 204.8MHz sampling clock. A simple change to the AD9528 configuration allows this frequency to be achieved with the 122.88MHz VCXO.
I create a profile as follows (I have also attached a zip of the files produced):

I also updated the device tree to accommodate these changes. I have attached the system_user.dtsi file.
When the Petalinux boots, I get the following error printed out:

I have attached the complete boot log.
Please can you provide guidelines on how I must set the configuration tool or how I must update my device tree settings to support my requested configuration.
I have seen other posts where customers have asked similar questions about the framer/deframer lane rate and the response was effectively 'try different frequencies until you find one that works'. Unfortunately that is not an option here because the frequencies are fixed so please can you provide guidelines on how I must configure the TX path so that the RX path can be operated at 204.8MHz. The RX path is currently the most important and so any changes needed to get the TX path to work will be fine for now.
Thank you.
/include/ "system-conf.dtsi"
/ {
// adrv9009_dac_fifo_bypass_s 35
// ad9528_reset_b, // 34
// ad9528_sysref_req, // 33
// adrv9009_reset_b, // 32 + 78
amba {
spi@ff040000 {
compatible = "cdns,spi-r1p6";
status = "okay";
is-decoded-cs = <0x0>;
num-cs = <0x3>;
clk0_ad9528: ad9528-1@1 {
compatible = "adi,ad9528";
reg = <1>;
#address-cells = <1>;
#size-cells = <0>;
spi-max-frequency = <10000000>;
//adi,spi-3wire-enable;
clock-output-names = "ad9528-1_out0", "ad9528-1_out1", "ad9528-1_out2",
"ad9528-1_out3", "ad9528-1_out4", "ad9528-1_out5", "ad9528-1_out6",
"ad9528-1_out7", "ad9528-1_out8", "ad9528-1_out9", "ad9528-1_out10",
"ad9528-1_out11", "ad9528-1_out12", "ad9528-1_out13";
#clock-cells = <1>;
adi,vcxo-freq = <122880000>;
adi,refa-enable;
adi,refa-diff-rcv-enable;
adi,refa-r-div = <1>;
adi,osc-in-cmos-neg-inp-enable;
// PLL1 config
adi,pll1-feedback-div = <4>;
adi,pll1-charge-pump-current-nA = <5000>;
// PLL2 config
adi,pll2-vco-div-m1 = <3>; // use 5 for 184320000 output device clock
adi,pll2-n2-div = <10>; // N / M1
adi,pll2-r1-div = <1>;
adi,pll2-charge-pump-current-nA = <805000>;
// SYSREF config
adi,sysref-src = <2>; // SYSREF_SRC_INTERNAL
adi,sysref-pattern-mode = <1>; // SYSREF_PATTERN_CONTINUOUS
adi,sysref-k-div = <512>;
adi,sysref-request-enable;
adi,sysref-nshot-mode = <3>; // SYSREF_NSHOT_4_PULSES
adi,sysref-request-trigger-mode = <0>; // SYSREF_LEVEL_HIGH
adi,rpole2 = <0>; // RPOLE2_900_OHM
adi,rzero = <7>; // RZERO_1850_OHM
adi,cpole1 = <2>; // CPOLE1_16_PF
adi,status-mon-pin0-function-select = <1>; // PLL1 & PLL2 Locked
adi,status-mon-pin1-function-select = <7>; // REFA Correct
reset-gpios = <&gpio 112 0>;
ad9528_0_c13: channel@13 {
reg = <13>;
adi,extended-name = "DEV_CLK";
adi,driver-mode = <0>; // DRIVER_MODE_LVDS
adi,divider-phase = <0>;
adi,channel-divider = <6>; // 204M8Hz <5>,
adi,signal-source = <0>; // SOURCE_VCO
};
ad9528_0_c1: channel@1 {
reg = <1>;
adi,extended-name = "FMC_CLK";
adi,driver-mode = <0>; // DRIVER_MODE_LVDS
adi,divider-phase = <0>;
adi,channel-divider = <6>; // 204M8Hz <5>,
adi,signal-source = <0>; // SOURCE_VCO
};
ad9528_0_c12: channel@12 {
reg = <12>;
adi,extended-name = "DEV_SYSREF";
adi,driver-mode = <0>; // DRIVER_MODE_LVDS
adi,divider-phase = <0>;
adi,channel-divider = <6>;// 204M8Hz <5>,
adi,signal-source = <2>; // SOURCE_SYSREF_VCO
};
ad9528_0_c3: channel@3 {
reg = <3>;
adi,extended-name = "FMC_SYSREF";
adi,driver-mode = <0>; // DRIVER_MODE_LVDS
adi,divider-phase = <0>;
adi,channel-divider = <6>;// 204M8Hz <5>,
adi,signal-source = <2>; // SOURCE_SYSREF_VCO
};
};
trx0_adrv9009: adrv9009-phy@0 {
compatible = "adrv9009";
reg = <0>;
#address-cells = <1>;
#size-cells = <0>;
// SPI Setup
spi-max-frequency = <25000000>;
reset-gpios = <&gpio 110 0>;
sysref-req-gpios = <&gpio 111 0>;
// Clocks
clocks = <&axi_adrv9009_rx_jesd_0>, <&axi_adrv9009_tx_jesd_0>,
<&axi_adrv9009_rx_os_jesd_0>, <&clk0_ad9528 13>,
<&clk0_ad9528 1>, <&clk0_ad9528 12>, <&clk0_ad9528 3>;
clock-names = "jesd_rx_clk", "jesd_tx_clk", "jesd_rx_os_clk",
"dev_clk", "fmc_clk", "sysref_dev_clk",
"sysref_fmc_clk";
clock-output-names = "rx_sampl_clk_0", "rx_os_sampl_clk_0", "tx_sampl_clk_0";
#clock-cells = <1>;
// JESD204
// JESD204 RX
adi,jesd204-framer-a-bank-id = <1>;
adi,jesd204-framer-a-device-id = <0>;
adi,jesd204-framer-a-lane0-id = <0>;
adi,jesd204-framer-a-m = <4>;
adi,jesd204-framer-a-k = <32>;
adi,jesd204-framer-a-f = <4>;
adi,jesd204-framer-a-np = <16>;
adi,jesd204-framer-a-scramble = <1>;
adi,jesd204-framer-a-external-sysref = <1>;
adi,jesd204-framer-a-serializer-lanes-enabled = <0x03>;
adi,jesd204-framer-a-serializer-lane-crossbar = <0xE4>;
adi,jesd204-framer-a-lmfc-offset = <31>;
adi,jesd204-framer-a-new-sysref-on-relink = <0>;
adi,jesd204-framer-a-syncb-in-select = <0>;
adi,jesd204-framer-a-over-sample = <0>;
adi,jesd204-framer-a-syncb-in-lvds-mode = <1>;
adi,jesd204-framer-a-syncb-in-lvds-pn-invert = <0>;
adi,jesd204-framer-a-enable-manual-lane-xbar = <0>;
// JESD204 OBS
adi,jesd204-framer-b-bank-id = <0>;
adi,jesd204-framer-b-device-id = <0>;
adi,jesd204-framer-b-lane0-id = <0>;
adi,jesd204-framer-b-m = <4>;
adi,jesd204-framer-b-k = <32>;
adi,jesd204-framer-b-f = <4>;
adi,jesd204-framer-b-np = <16>;
adi,jesd204-framer-b-scramble = <1>;
adi,jesd204-framer-b-external-sysref = <1>;
adi,jesd204-framer-b-serializer-lanes-enabled = <0x0C>;
adi,jesd204-framer-b-serializer-lane-crossbar = <0xE4>;
adi,jesd204-framer-b-lmfc-offset = <31>;
adi,jesd204-framer-b-new-sysref-on-relink = <0>;
adi,jesd204-framer-b-syncb-in-select = <1>;
adi,jesd204-framer-b-over-sample = <0>;
adi,jesd204-framer-b-syncb-in-lvds-mode = <1>;
adi,jesd204-framer-b-syncb-in-lvds-pn-invert = <0>;
adi,jesd204-framer-b-enable-manual-lane-xbar = <0>;
// JESD204 TX
adi,jesd204-deframer-a-bank-id = <0>;
adi,jesd204-deframer-a-device-id = <0>;
adi,jesd204-deframer-a-lane0-id = <0>;
adi,jesd204-deframer-a-m = <4>;
adi,jesd204-deframer-a-k = <32>;
adi,jesd204-deframer-a-scramble = <1>;
adi,jesd204-deframer-a-external-sysref = <1>;
adi,jesd204-deframer-a-deserializer-lanes-enabled = <0x0F>;
adi,jesd204-deframer-a-deserializer-lane-crossbar = <0xE4>;
adi,jesd204-deframer-a-lmfc-offset = <17>;
adi,jesd204-deframer-a-new-sysref-on-relink = <0>;
adi,jesd204-deframer-a-syncb-out-select = <0>;
adi,jesd204-deframer-a-np = <16>;
adi,jesd204-deframer-a-syncb-out-lvds-mode = <1>;
adi,jesd204-deframer-a-syncb-out-lvds-pn-invert = <0>;
adi,jesd204-deframer-a-syncb-out-cmos-slew-rate = <0>;
adi,jesd204-deframer-a-syncb-out-cmos-drive-level = <0>;
adi,jesd204-deframer-a-enable-manual-lane-xbar = <0>;
adi,jesd204-ser-amplitude = <15>;
adi,jesd204-ser-pre-emphasis = <1>;
adi,jesd204-ser-invert-lane-polarity = <0>;
adi,jesd204-des-invert-lane-polarity = <0>;
adi,jesd204-des-eq-setting = <1>;
adi,jesd204-sysref-lvds-mode = <1>;
adi,jesd204-sysref-lvds-pn-invert = <0>;
// RX
adi,rx-profile-rx-fir-gain_db = <(-6)>;
adi,rx-profile-rx-fir-num-fir-coefs = <48>;
// 204M8Hz adi,rx-profile-rx-fir-coefs = /bits/ 16 <(-2) (23) (46) (-17) (-104) (10) (208) (23) (-370) (-97) (607) (240) (-942) (-489) (1407) (910) (-2065) (-1637) (3058) (2995) (-4912) (-6526) (9941) (30489) (30489) (9941) (-6526) (-4912) (2995) (3058) (-1637) (-2065) (910) (1407) (-489) (-942) (240) (607) (-97) (-370) (23) (208) (10) (-104) (-17) (46) (23) (-2)>;
adi,rx-profile-rx-fir-coefs = /bits/ 16 <(-7) (-25) (32) (52) (-69) (-114) (142) (211) (-254) (-365) (430) (594) (-688) (-932) (1068) (1435) (-1638) (-2231) (2546) (3638) (-4326) (-7191) (9305) (31150) (31150) (9305) (-7191) (-4326) (3638) (2546) (-2231) (-1638) (1435) (1068) (-932) (-688) (594) (430) (-365) (-254) (211) (142) (-114) (-69) (52) (32) (-25) (-7)>;
adi,rx-profile-rx-fir-decimation = <2>;
adi,rx-profile-rx-dec5-decimation = <4>;
adi,rx-profile-rhb1-decimation = <1>;
adi,rx-profile-rx-output-rate_khz = <204800>; // 204M8Hz <245760>;
adi,rx-profile-rf-bandwidth_hz = <167000000>; // 204M8Hz <200000000>;
adi,rx-profile-rx-bbf3d-bcorner_khz = <167000>; // 204M8Hz <200000>;
// 204M8Hz adi,rx-profile-rx-adc-profile = /bits/ 16 <182 142 173 90 1280 982 1335 96 1369 48 1012 18 48 48 37 208 0 0 0 0 52 0 7 6 42 0 7 6 42 0 25 27 0 0 25 27 0 0 165 44 31 905>;
adi,rx-profile-rx-adc-profile = /bits/ 16 <222 168 181 90 1280 945 1321 90 1197 40 844 19 48 42 31 212 0 0 0 0 53 0 7 6 42 0 7 6 42 0 25 27 0 0 25 27 0 0 165 44 31 905>;
adi,rx-profile-rx-ddc-mode = <0>;
adi,rx-nco-shifter-band-a-input-band-width_khz = <0>;
adi,rx-nco-shifter-band-a-input-center-freq_khz = <0>;
adi,rx-nco-shifter-band-a-nco1-freq_khz = <0>;
adi,rx-nco-shifter-band-a-nco2-freq_khz = <0>;
adi,rx-nco-shifter-band-binput-band-width_khz = <0>;
adi,rx-nco-shifter-band-binput-center-freq_khz = <0>;
adi,rx-nco-shifter-band-bnco1-freq_khz = <0>;
adi,rx-nco-shifter-band-bnco2-freq_khz = <0>;
adi,rx-gain-control-gain-mode = <0>;
adi,rx-gain-control-rx1-gain-index = <255>;
adi,rx-gain-control-rx2-gain-index = <255>;
adi,rx-gain-control-rx1-max-gain-index = <255>;
adi,rx-gain-control-rx1-min-gain-index = <195>;
adi,rx-gain-control-rx2-max-gain-index = <255>;
adi,rx-gain-control-rx2-min-gain-index = <195>;
adi,rx-settings-framer-sel = <0>;
adi,rx-settings-rx-channels = <3>;
// ORX
adi,orx-profile-rx-fir-gain_db = <(-6)>; // 204M8Hz <6>;
adi,orx-profile-rx-fir-num-fir-coefs = <48>; // 204M8Hz <24>;
// 204M8Hz adi,orx-profile-rx-fir-coefs = /bits/ 16 <(-10) (7) (-10) (-12) (6) (-12) (16) (-16) (1) (63) (-431) (17235) (-431) (63) (1) (-16) (16) (-12) (6) (-12) (-10) (7) (-10) (0)>;
adi,orx-profile-rx-fir-coefs = /bits/ 16 <(-8) (-21) (30) (48) (-65) (-104) (119) (161) (-265) (-327) (424) (538) (-668) (-849) (1030) (1309) (-1576) (-2038) (2460) (3343) (-4182) (-6560) (9503) (30461) (30461) (9503) (-6560) (-4182) (3343) (2460) (-2038) (-1576) (1309) (1030) (-849) (-668) (538) (424) (-327) (-265) (161) (119) (-104) (-65) (48) (30) (-21) (-8)>;
adi,orx-profile-rx-fir-decimation = <2>; // 204M8Hz <1>;
adi,orx-profile-rx-dec5-decimation = <4>;
adi,orx-profile-rhb1-decimation = <1>; // 204M8Hz <2>;
adi,orx-profile-orx-output-rate_khz = <204800>; // 204M8Hz <245760>;
adi,orx-profile-rf-bandwidth_hz = <167000000>; // 204M8Hz <200000000>;
adi,orx-profile-rx-bbf3d-bcorner_khz = <225000>;
// 204M8Hz adi,orx-profile-orx-low-pass-adc-profile = /bits/ 16 <185 141 172 90 1280 942 1332 90 1368 46 1016 19 48 48 37 208 0 0 0 0 52 0 7 6 42 0 7 6 42 0 25 27 0 0 25 27 0 0 165 44 31 905>;
adi,orx-profile-orx-low-pass-adc-profile = /bits/ 16 <222 168 181 90 1280 945 1321 90 1197 40 844 19 48 42 31 212 0 0 0 0 53 0 7 6 42 0 7 6 42 0 25 27 0 0 25 27 0 0 165 44 31 905>;
// 204M8Hz adi,orx-profile-orx-band-pass-adc-profile = /bits/ 16 <0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0>;
adi,orx-profile-orx-band-pass-adc-profile = /bits/ 16 <222 168 181 90 1280 945 1321 90 1197 40 844 19 48 42 31 212 0 0 0 0 53 0 7 6 42 0 7 6 42 0 25 27 0 0 25 27 0 0 165 44 31 905>;
adi,orx-profile-orx-ddc-mode = <0>;
adi,orx-profile-orx-merge-filter = /bits/ 16 <0 0 0 0 0 0 0 0 0 0 0 0>;
adi,orx-gain-control-gain-mode = <0>;
adi,orx-gain-control-orx1-gain-index = <255>;
adi,orx-gain-control-orx2-gain-index = <255>;
adi,orx-gain-control-orx1-max-gain-index = <255>;
adi,orx-gain-control-orx1-min-gain-index = <195>;
adi,orx-gain-control-orx2-max-gain-index = <255>;
adi,orx-gain-control-orx2-min-gain-index = <195>;
adi,obs-settings-framer-sel = <1>;
adi,obs-settings-obs-rx-channels-enable = <3>;
adi,obs-settings-obs-rx-lo-source = <0>;
// TX
adi,tx-profile-tx-fir-gain_db = <0>; // 204M8Hz <6>;
adi,tx-profile-tx-fir-num-fir-coefs = <20>; // 204M8Hz <40>;
// 204M8Hz adi,tx-profile-tx-fir-coefs = /bits/ 16 <(-14) (5) (-9) (6) (-4) (19) (-29) (27) (-30) (46) (-63) (77) (-103) (150) (-218) (337) (-599) (1266) (-2718) (19537) (-2718) (1266) (-599) (337) (-218) (150) (-103) (77) (-63) (46) (-30) (27) (-29) (19) (-4) (6) (-9) (5) (-14) (0)>;
adi,tx-profile-tx-fir-coefs = /bits/ 16 <(0) (0) (0) (0) (0) (0) (0) (0) (0) (0) (0) (0) (0) (0) (0) (0) (0) (0) (0) (0)>;
adi,tx-profile-dac-div = <1>;
adi,tx-profile-tx-fir-interpolation = <1>;
adi,tx-profile-thb1-interpolation = <2>;
adi,tx-profile-thb2-interpolation = <2>;
adi,tx-profile-thb3-interpolation = <2>;
adi,tx-profile-tx-int5-interpolation = <1>;
adi,tx-profile-tx-input-rate_khz = <204800>; // 204M8Hz <245760>;
adi,tx-profile-primary-sig-bandwidth_hz = <75000000>; // 204M8Hz <100000000>;
adi,tx-profile-rf-bandwidth_hz = <167000000>; // 204M8Hz <225000000>;
adi,tx-profile-tx-dac3d-bcorner_khz = <200000>; // 204M8Hz <225000>;
adi,tx-profile-tx-bbf3d-bcorner_khz = <100000>; // 204M8Hz <113000>;
adi,tx-profile-loop-back-adc-profile = /bits/ 16 <206 132 168 90 1280 641 1307 53 1359 28 1039 30 48 48 37 210 0 0 0 0 53 0 7 6 42 0 7 6 42 0 25 27 0 0 25 27 0 0 165 44 31 905>;
adi,tx-settings-deframer-sel = <0>;
adi,tx-settings-tx-channels = <3>;
adi,tx-settings-tx-atten-step-size = <0>;
adi,tx-settings-tx1-atten_md-b = <10000>;
adi,tx-settings-tx2-atten_md-b = <10000>;
adi,tx-settings-dis-tx-data-if-pll-unlock = <0>;
// Clocks
adi,dig-clocks-device-clock_khz = <204800>; // 204M8Hz <245760>;
adi,dig-clocks-clk-pll-vco-freq_khz = <8192000>; // 204M8Hz <9830400>;
adi,dig-clocks-clk-pll-hs-div = <1>;
adi,dig-clocks-rf-pll-use-external-lo = <0>;
adi,dig-clocks-rf-pll-phase-sync-mode = <0>;
// AGC
adi,rxagc-peak-agc-under-range-low-interval_ns = <205>;
adi,rxagc-peak-agc-under-range-mid-interval = <2>;
adi,rxagc-peak-agc-under-range-high-interval = <4>;
adi,rxagc-peak-apd-high-thresh = <39>;
adi,rxagc-peak-apd-low-gain-mode-high-thresh = <36>;
adi,rxagc-peak-apd-low-thresh = <23>;
adi,rxagc-peak-apd-low-gain-mode-low-thresh = <19>;
adi,rxagc-peak-apd-upper-thresh-peak-exceeded-cnt = <6>;
adi,rxagc-peak-apd-lower-thresh-peak-exceeded-cnt = <3>;
adi,rxagc-peak-apd-gain-step-attack = <4>;
adi,rxagc-peak-apd-gain-step-recovery = <2>;
adi,rxagc-peak-enable-hb2-overload = <1>;
adi,rxagc-peak-hb2-overload-duration-cnt = <1>;
adi,rxagc-peak-hb2-overload-thresh-cnt = <4>;
adi,rxagc-peak-hb2-high-thresh = <181>;
adi,rxagc-peak-hb2-under-range-low-thresh = <45>;
adi,rxagc-peak-hb2-under-range-mid-thresh = <90>;
adi,rxagc-peak-hb2-under-range-high-thresh = <128>;
adi,rxagc-peak-hb2-upper-thresh-peak-exceeded-cnt = <6>;
adi,rxagc-peak-hb2-lower-thresh-peak-exceeded-cnt = <3>;
adi,rxagc-peak-hb2-gain-step-high-recovery = <2>;
adi,rxagc-peak-hb2-gain-step-low-recovery = <4>;
adi,rxagc-peak-hb2-gain-step-mid-recovery = <8>;
adi,rxagc-peak-hb2-gain-step-attack = <4>;
adi,rxagc-peak-hb2-overload-power-mode = <1>;
adi,rxagc-peak-hb2-ovrg-sel = <0>;
adi,rxagc-peak-hb2-thresh-config = <3>;
adi,rxagc-power-power-enable-measurement = <1>;
adi,rxagc-power-power-use-rfir-out = <1>;
adi,rxagc-power-power-use-bbdc2 = <0>;
adi,rxagc-power-under-range-high-power-thresh = <9>;
adi,rxagc-power-under-range-low-power-thresh = <2>;
adi,rxagc-power-under-range-high-power-gain-step-recovery = <4>;
adi,rxagc-power-under-range-low-power-gain-step-recovery = <4>;
adi,rxagc-power-power-measurement-duration = <5>;
adi,rxagc-power-rx1-tdd-power-meas-duration = <5>;
adi,rxagc-power-rx1-tdd-power-meas-delay = <1>;
adi,rxagc-power-rx2-tdd-power-meas-duration = <5>;
adi,rxagc-power-rx2-tdd-power-meas-delay = <1>;
adi,rxagc-power-upper0-power-thresh = <2>;
adi,rxagc-power-upper1-power-thresh = <0>;
adi,rxagc-power-power-log-shift = <0>;
adi,rxagc-agc-peak-wait-time = <4>;
adi,rxagc-agc-rx1-max-gain-index = <255>;
adi,rxagc-agc-rx1-min-gain-index = <195>;
adi,rxagc-agc-rx2-max-gain-index = <255>;
adi,rxagc-agc-rx2-min-gain-index = <195>;
adi,rxagc-agc-gain-update-counter_us = <250>;
adi,rxagc-agc-rx1-attack-delay = <10>;
adi,rxagc-agc-rx2-attack-delay = <10>;
adi,rxagc-agc-slow-loop-settling-delay = <16>;
adi,rxagc-agc-low-thresh-prevent-gain = <0>;
adi,rxagc-agc-change-gain-if-thresh-high = <1>;
adi,rxagc-agc-peak-thresh-gain-control-mode = <1>;
adi,rxagc-agc-reset-on-rxon = <0>;
adi,rxagc-agc-enable-sync-pulse-for-gain-counter = <0>;
adi,rxagc-agc-enable-ip3-optimization-thresh = <0>;
adi,rxagc-ip3-over-range-thresh = <31>;
adi,rxagc-ip3-over-range-thresh-index = <246>;
adi,rxagc-ip3-peak-exceeded-cnt = <4>;
adi,rxagc-agc-enable-fast-recovery-loop = <0>;
// Misc
adi,aux-dac-enables = <0x00>; // Mask
adi,aux-dac-vref0 = <3>;
adi,aux-dac-resolution0 = <0>;
adi,aux-dac-values0 = <0>;
adi,aux-dac-vref1 = <3>;
adi,aux-dac-resolution1 = <0>;
adi,aux-dac-values1 = <0>;
adi,aux-dac-vref2 = <3>;
adi,aux-dac-resolution2 = <0>;
adi,aux-dac-values2 = <0>;
adi,aux-dac-vref3 = <3>;
adi,aux-dac-resolution3 = <0>;
adi,aux-dac-values3 = <0>;
adi,aux-dac-vref4 = <3>;
adi,aux-dac-resolution4 = <0>;
adi,aux-dac-values4 = <0>;
adi,aux-dac-vref5 = <3>;
adi,aux-dac-resolution5 = <0>;
adi,aux-dac-values5 = <0>;
adi,aux-dac-vref6 = <3>;
adi,aux-dac-resolution6 = <0>;
adi,aux-dac-values6 = <0>;
adi,aux-dac-vref7 = <3>;
adi,aux-dac-resolution7 = <0>;
adi,aux-dac-values7 = <0>;
adi,aux-dac-vref8 = <3>;
adi,aux-dac-resolution8 = <0>;
adi,aux-dac-values8 = <0>;
adi,aux-dac-vref9 = <3>;
adi,aux-dac-resolution9 = <0>;
adi,aux-dac-values9 = <0>;
adi,aux-dac-vref10 = <3>;
adi,aux-dac-resolution10 = <0>;
adi,aux-dac-values10 = <0>;
adi,aux-dac-vref11 = <3>;
adi,aux-dac-resolution11 = <0>;
adi,aux-dac-values11 = <0>;
adi,arm-gpio-config-orx1-tx-sel0-pin-gpio-pin-sel = <0>;
adi,arm-gpio-config-orx1-tx-sel0-pin-polarity = <0>;
adi,arm-gpio-config-orx1-tx-sel0-pin-enable = <0>;
adi,arm-gpio-config-orx1-tx-sel1-pin-gpio-pin-sel = <0>;
adi,arm-gpio-config-orx1-tx-sel1-pin-polarity = <0>;
adi,arm-gpio-config-orx1-tx-sel1-pin-enable = <0>;
adi,arm-gpio-config-orx2-tx-sel0-pin-gpio-pin-sel = <0>;
adi,arm-gpio-config-orx2-tx-sel0-pin-polarity = <0>;
adi,arm-gpio-config-orx2-tx-sel0-pin-enable = <0>;
adi,arm-gpio-config-orx2-tx-sel1-pin-gpio-pin-sel = <0>;
adi,arm-gpio-config-orx2-tx-sel1-pin-polarity = <0>;
adi,arm-gpio-config-orx2-tx-sel1-pin-enable = <0>;
adi,arm-gpio-config-en-tx-tracking-cals-gpio-pin-sel = <0>;
adi,arm-gpio-config-en-tx-tracking-cals-polarity = <0>;
adi,arm-gpio-config-en-tx-tracking-cals-enable = <0>;
adi,orx-lo-cfg-disable-aux-pll-relocking = <0>;
adi,orx-lo-cfg-gpio-select = <19>;
adi,fhm-config-fhm-gpio-pin = <0>;
adi,fhm-config-fhm-min-freq_mhz = <2400>;
adi,fhm-config-fhm-max-freq_mhz = <2500>;
adi,fhm-mode-fhm-enable = <0>;
adi,fhm-mode-enable-mcs-sync = <0>;
adi,fhm-mode-fhm-trigger-mode = <0>;
adi,fhm-mode-fhm-exit-mode = <1>;
adi,fhm-mode-fhm-init-frequency_hz = <2450000000>;
adi,rx1-gain-ctrl-pin-inc-step = <1>;
adi,rx1-gain-ctrl-pin-dec-step = <1>;
adi,rx1-gain-ctrl-pin-rx-gain-inc-pin = <0>;
adi,rx1-gain-ctrl-pin-rx-gain-dec-pin = <1>;
adi,rx1-gain-ctrl-pin-enable = <0>;
adi,rx2-gain-ctrl-pin-inc-step = <1>;
adi,rx2-gain-ctrl-pin-dec-step = <1>;
adi,rx2-gain-ctrl-pin-rx-gain-inc-pin = <3>;
adi,rx2-gain-ctrl-pin-rx-gain-dec-pin = <4>;
adi,rx2-gain-ctrl-pin-enable = <0>;
adi,tx1-atten-ctrl-pin-step-size = <0>;
adi,tx1-atten-ctrl-pin-tx-atten-inc-pin = <4>;
adi,tx1-atten-ctrl-pin-tx-atten-dec-pin = <5>;
adi,tx1-atten-ctrl-pin-enable = <0>;
adi,tx2-atten-ctrl-pin-step-size = <0>;
adi,tx2-atten-ctrl-pin-tx-atten-inc-pin = <6>;
adi,tx2-atten-ctrl-pin-tx-atten-dec-pin = <7>;
adi,tx2-atten-ctrl-pin-enable = <0>;
adi,tx-pa-protection-avg-duration = <3>;
adi,tx-pa-protection-tx-atten-step = <2>;
adi,tx-pa-protection-tx1-power-threshold = <4096>;
adi,tx-pa-protection-tx2-power-threshold = <4096>;
adi,tx-pa-protection-peak-count = <4>;
adi,tx-pa-protection-tx1-peak-threshold = <140>;
adi,tx-pa-protection-tx2-peak-threshold = <140>;
};
amba_pl@0 {
interrupt-parent = <&gic>;
#address-cells = <0x2>;
#size-cells = <0x2>;
compatible = "simple-bus";
ranges;
/delete-node/ axi_adrv9009@a00c0000;
/delete-node/ axi_dmac@a0100000;
/delete-node/ axi_dmac@a0120000;
/delete-node/ axi_dmac@a0140000;
axi_intc: interrupt-controller@a000f000 {
#interrupt-cells = <0x2>;
compatible = "xlnx,xps-intc-1.00.a";
interrupt-controller;
};
rx_dma_0: dma@a0140000 {
compatible = "adi,axi-dmac-1.00.a";
reg = <0x0 0xa0140000 0x0 0x10000>;
#dma-cells = <1>;
#clock-cells = <0>;
interrupt-parent = <&axi_intc>;
interrupts = <0x5 0x2>;
clocks = <&clk 72>;
adi,channels {
#size-cells = <0>;
#address-cells = <1>;
dma-channel@0 {
reg = <0>;
adi,source-bus-width = <64>;
adi,source-bus-type = <2>;
adi,destination-bus-width = <64>;
adi,destination-bus-type = <0>;
};
};
};
rx_obs_dma_0: dma@a0120000 {
compatible = "adi,axi-dmac-1.00.a";
reg = <0x0 0xa0120000 0x0 0x10000>;
#dma-cells = <1>;
#clock-cells = <0>;
interrupt-parent = <&axi_intc>;
interrupts = <0x3 0x2>;
clocks = <&clk 72>;
adi,channels {
#size-cells = <0>;
#address-cells = <1>;
dma-channel@0 {
reg = <0>;
adi,source-bus-width = <128>;
adi,source-bus-type = <2>;
adi,destination-bus-width = <64>;
adi,destination-bus-type = <0>;
};
};
};
tx_dma_0: dma@a0100000 {
compatible = "adi,axi-dmac-1.00.a";
reg = <0x0 0xa0100000 0x0 0x10000>;
#dma-cells = <1>;
#clock-cells = <0>;
interrupt-parent = <&axi_intc>;
interrupts = <0x4 0x2>;
clocks = <&clk 72>;
adi,channels {
#size-cells = <0>;
#address-cells = <1>;
dma-channel@0 {
reg = <0>;
adi,source-bus-width = <128>;
adi,source-bus-type = <0>;
adi,destination-bus-width = <128>;
adi,destination-bus-type = <2>;
};
};
};
axi_adrv9009_core_rx_0: axi-adrv9009-rx-hpc@a00c0000 {
compatible = "adi,axi-adrv9009-rx-1.0";
reg = <0x0 0xa00c0000 0x0 0x8000>;
dmas = <&rx_dma_0 0>;
dma-names = "rx";
spibus-connected = <&trx0_adrv9009>;
};
axi_adrv9009_core_rx_obs_0: axi-adrv9009-rx-obs-hpc@a00c8000 {
compatible = "adi,axi-adrv9009-obs-1.0";
reg = <0x0 0xa00c8000 0x0 0x1000>;
dmas = <&rx_obs_dma_0 0>;
dma-names = "rx";
clocks = <&trx0_adrv9009 1>;
clock-names = "sampl_clk";
};
axi_adrv9009_core_tx_0: axi-adrv9009-tx-hpc@a00c4000 {
compatible = "adi,axi-adrv9009-tx-1.0";
reg = <0x0 0xa00c4000 0x0 0x4000>;
dmas = <&tx_dma_0 0>;
dma-names = "tx";
clocks = <&trx0_adrv9009 2>;
clock-names = "sampl_clk";
spibus-connected = <&trx0_adrv9009>;
//adi,axi-pl-fifo-enable;
plddrbypass-gpios = <&gpio 113 0>;
};
axi_adrv9009_rx_jesd_0: axi_jesd204_rx@a0014000 {
compatible = "adi,axi-jesd204-rx-1.0";
reg = <0x0 0xa0014000 0x0 0x4000>;
clocks = <&clk 71>, <&axi_adrv9009_adxcvr_rx_0 1>, <&axi_adrv9009_adxcvr_rx_0 0>;
clock-names = "s_axi_aclk", "device_clk", "lane_clk";
#clock-cells = <0>;
clock-output-names = "jesd_rx_lane_clk";
adi,octets-per-frame = <4>;
adi,frames-per-multiframe = <32>;
};
axi_adrv9009_tx_jesd_0: axi_jesd204_tx@a001c000 {
compatible = "adi,axi-jesd204-tx-1.0";
reg = <0x0 0xa001c000 0x0 0x4000>;
clocks = <&clk 71>, <&axi_adrv9009_adxcvr_tx_0 1>, <&axi_adrv9009_adxcvr_tx_0 0>;
clock-names = "s_axi_aclk", "device_clk", "lane_clk";
#clock-cells = <0>;
clock-output-names = "jesd_tx_lane_clk";
adi,octets-per-frame = <2>;
adi,frames-per-multiframe = <32>;
adi,converter-resolution = <14>;
adi,bits-per-sample = <16>;
adi,converters-per-device = <4>;
adi,control-bits-per-sample = <2>;
};
axi_adrv9009_rx_os_jesd_0: axi_jesd204_rx@a0018000 {
compatible = "adi,axi-jesd204-rx-1.0";
reg = <0x0 0xa0018000 0x0 0x4000>;
clocks = <&clk 71>, <&axi_adrv9009_adxcvr_rx_os_0 1>, <&axi_adrv9009_adxcvr_rx_os_0 0>;
clock-names = "s_axi_aclk", "device_clk", "lane_clk";
#clock-cells = <0>;
clock-output-names = "jesd_rx_os_lane_clk";
adi,octets-per-frame = <4>;
adi,frames-per-multiframe = <32>;
};
axi_adrv9009_adxcvr_rx_0: axi_adxcvr@a0090000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "adi,axi-adxcvr-1.0";
reg = <0x0 0xa0090000 0x0 0x10000>;
clocks = <&clk0_ad9528 1>;
clock-names = "conv";
#clock-cells = <1>;
clock-output-names = "rx_gt_clk", "rx_out_clk";
adi,sys-clk-select = <0>;
adi,out-clk-select = <3>;
adi,use-lpm-enable;
adi,use-cpll-enable;
};
axi_adrv9009_adxcvr_rx_os_0: axi_adxcvr@a0080000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "adi,axi-adxcvr-1.0";
reg = <0x0 0xa0080000 0x0 0x10000>;
clocks = <&clk0_ad9528 1>;
clock-names = "conv";
#clock-cells = <1>;
clock-output-names = "rx_os_gt_clk", "rx_os_out_clk";
adi,sys-clk-select = <0>;
adi,out-clk-select = <3>;
adi,use-lpm-enable;
adi,use-cpll-enable;
};
axi_adrv9009_adxcvr_tx_0: axi_adxcvr@a00b0000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "adi,axi-adxcvr-1.0";
reg = <0x0 0xa00b0000 0x0 0x10000>;
clocks = <&clk0_ad9528 1>;
clock-names = "conv";
#clock-cells = <1>;
clock-output-names = "tx_gt_clk", "tx_out_clk";
adi,sys-clk-select = <3>;
adi,out-clk-select = <3>;
};
};
};
øXilinx Zynq MP First Stage Boot Loader
Release 2018.2 Oct 21 2020 - 15:24:51
Disabling ETH1 and enabling USB PHY 1.
PE1 TEST PLATFORM: Fixed MAC address.
Serial number: 1193046.
MAC address: 0:A:35:12:34:56
NOTICE: ATF running on XCZU6EG/silicon v4/RTL5.1 at 0xfffea000
NOTICE: BL31: Secure code at 0x0
NOTICE: BL31: Non secure code at 0x8000000
NOTICE: BL31: v1.4(release):xilinx-v2018.1-4-g93a69a5a
NOTICE: BL31: Built : 11:29:44, Feb 9 2021
PMUFW: v1.0
U-Boot 2018.01 (Feb 09 2021 - 13:31:04 +0200) Xilinx ZynqMP ZCU102 rev1.0
I2C: ready
DRAM: 2 GiB
usb dr_mode not found
EL Level: EL2
Chip ID: zu6eg
MMC: sdhci@ff160000: 0 (eMMC), sdhci@ff170000: 1 (SD)
Invalid bus 0 (err=-19)
*** Warning - spi_flash_probe_bus_cs() failed, using default environment
In: serial@ff000000
Out: serial@ff000000
Err: serial@ff000000
Board: Xilinx ZynqMP
Bootmode: SD_MODE1
Net: ZYNQ GEM: ff0b0000, phyaddr 3, interface rgmii-id
PHY is not detected
GEM PHY init failed
No ethernet found.
U-BOOT for frm127101u1r1
## Info: input data size = 27 = 0x1B
Hit any key to stop autoboot: 0
Device: sdhci@ff160000
Manufacturer ID: 70
OEM: 100
Name: W5251
Tran Speed: 200000000
Rd Block Len: 512
MMC version 5.0
High Capacity: Yes
Capacity: 14.3 GiB
Bus Width: 4-bit
Erase Group Size: 512 KiB
HC WP Group Size: 16 MiB
User Capacity: 14.3 GiB
Boot Capacity: 4 MiB ENH
RPMB Capacity: 4 MiB ENH
reading image.ub
20455512 bytes read in 1355 ms (14.4 MiB/s)
## Loading kernel from FIT Image at 10000000 ...
Using 'conf@system-top.dtb' configuration
Trying 'kernel@1' kernel subimage
Description: Linux kernel
Type: Kernel Image
Compression: gzip compressed
Data Start: 0x100000f8
Data Size: 7593972 Bytes = 7.2 MiB
Architecture: AArch64
OS: Linux
Load Address: 0x00080000
Entry Point: 0x00080000
Hash algo: sha1
Hash value: 23112b67bbc85a752687fffcd2d4ce69dc4f6b19
Verifying Hash Integrity ... sha1+ OK
## Loading ramdisk from FIT Image at 10000000 ...
Using 'conf@system-top.dtb' configuration
Trying 'ramdisk@1' ramdisk subimage
Description: petalinux-user-image
Type: RAMDisk Image
Compression: gzip compressed
Data Start: 0x10750b18
Data Size: 12783536 Bytes = 12.2 MiB
Architecture: AArch64
OS: Linux
Load Address: unavailable
Entry Point: unavailable
Hash algo: sha1
Hash value: 79f2b9d0003de9d3907f0af9ca8343d65b5921ab
Verifying Hash Integrity ... sha1+ OK
## Loading fdt from FIT Image at 10000000 ...
Using 'conf@system-top.dtb' configuration
Trying 'fdt@system-top.dtb' fdt subimage
Description: Flattened Device Tree blob
Type: Flat Device Tree
Compression: uncompressed
Data Start: 0x1073e1f0
Data Size: 75875 Bytes = 74.1 KiB
Architecture: AArch64
Hash algo: sha1
Hash value: 3b5f196cea86388bbfe1cefd50b9d8a360481ba5
Verifying Hash Integrity ... sha1+ OK
Booting using the fdt blob at 0x1073e1f0
ZYNQ GEM: ff0b0000, phyaddr 3, interface rgmii-id
mdio_register: non unique device name 'eth0'
Uncompressing Kernel Image ... OK
Loading Ramdisk to 073cf000, end 07ffffb0 ... OK
Loading Device Tree to 00000000073b9000, end 00000000073ce862 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.0 (oe-user@oe-host) (gcc version 7.2.0 (GCC)) #1 SMP Wed Nov 4 14:42:27 SAST 2020
[ 0.000000] Boot CPU: AArch64 Processor [410fd034]
[ 0.000000] Machine model: xlnx,zynqmp
[ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
[ 0.000000] bootconsole [cdns0] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 256 MiB at 0x000000006fc00000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] random: fast init done
[ 0.000000] percpu: Embedded 21 pages/cpu @ffffffc06fb55000 s45080 r8192 d32744 u86016
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: enabling workaround for ARM erratum 845719
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516110
[ 0.000000] Kernel command line: earlycon clk_ignore_unused cpuidle.off=1 uio_pdrv_genirq.of_id="generic-uio"
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes)
[ 0.000000] Memory: 1767384K/2093056K available (10428K kernel code, 710K rwdata, 4632K rodata, 512K init, 2158K bss, 63528K reserved, 262144K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffffff8000000000 - 0xffffff8008000000 ( 128 MB)
[ 0.000000] vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000 ( 250 GB)
[ 0.000000] .text : 0xffffff8008080000 - 0xffffff8008ab0000 ( 10432 KB)
[ 0.000000] .rodata : 0xffffff8008ab0000 - 0xffffff8008f40000 ( 4672 KB)
[ 0.000000] .init : 0xffffff8008f40000 - 0xffffff8008fc0000 ( 512 KB)
[ 0.000000] .data : 0xffffff8008fc0000 - 0xffffff8009071a00 ( 711 KB)
[ 0.000000] .bss : 0xffffff8009071a00 - 0xffffff800928d330 ( 2159 KB)
[ 0.000000] fixed : 0xffffffbefe7fd000 - 0xffffffbefec00000 ( 4108 KB)
[ 0.000000] PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000 ( 16 MB)
[ 0.000000] vmemmap : 0xffffffbf00000000 - 0xffffffc000000000 ( 4 GB maximum)
[ 0.000000] 0xffffffbf00000000 - 0xffffffbf01bf2000 ( 27 MB actual)
[ 0.000000] memory : 0xffffffc000000000 - 0xffffffc07fc00000 ( 2044 MB)
[ 0.000000] Hierarchical RCU implementation.
[ 0.000000] RCU event tracing is enabled.
[ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] irq-xilinx: /amba_pl@0/interrupt-controller@a000f000: num_irq=6, edge=0x0
[ 0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171015c90f, max_idle_ns: 440795203080 ns
[ 0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns
[ 0.008297] Console: colour dummy device 80x25
[ 0.012550] console [tty0] enabled
[ 0.015915] bootconsole [cdns0] disabled
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.0 (oe-user@oe-host) (gcc version 7.2.0 (GCC)) #1 SMP Wed Nov 4 14:42:27 SAST 2020
[ 0.000000] Boot CPU: AArch64 Processor [410fd034]
[ 0.000000] Machine model: xlnx,zynqmp
[ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
[ 0.000000] bootconsole [cdns0] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 256 MiB at 0x000000006fc00000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] random: fast init done
[ 0.000000] percpu: Embedded 21 pages/cpu @ffffffc06fb55000 s45080 r8192 d32744 u86016
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: enabling workaround for ARM erratum 845719
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516110
[ 0.000000] Kernel command line: earlycon clk_ignore_unused cpuidle.off=1 uio_pdrv_genirq.of_id="generic-uio"
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes)
[ 0.000000] Memory: 1767384K/2093056K available (10428K kernel code, 710K rwdata, 4632K rodata, 512K init, 2158K bss, 63528K reserved, 262144K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffffff8000000000 - 0xffffff8008000000 ( 128 MB)
[ 0.000000] vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000 ( 250 GB)
[ 0.000000] .text : 0xffffff8008080000 - 0xffffff8008ab0000 ( 10432 KB)
[ 0.000000] .rodata : 0xffffff8008ab0000 - 0xffffff8008f40000 ( 4672 KB)
[ 0.000000] .init : 0xffffff8008f40000 - 0xffffff8008fc0000 ( 512 KB)
[ 0.000000] .data : 0xffffff8008fc0000 - 0xffffff8009071a00 ( 711 KB)
[ 0.000000] .bss : 0xffffff8009071a00 - 0xffffff800928d330 ( 2159 KB)
[ 0.000000] fixed : 0xffffffbefe7fd000 - 0xffffffbefec00000 ( 4108 KB)
[ 0.000000] PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000 ( 16 MB)
[ 0.000000] vmemmap : 0xffffffbf00000000 - 0xffffffc000000000 ( 4 GB maximum)
[ 0.000000] 0xffffffbf00000000 - 0xffffffbf01bf2000 ( 27 MB actual)
[ 0.000000] memory : 0xffffffc000000000 - 0xffffffc07fc00000 ( 2044 MB)
[ 0.000000] Hierarchical RCU implementation.
[ 0.000000] RCU event tracing is enabled.
[ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] irq-xilinx: /amba_pl@0/interrupt-controller@a000f000: num_irq=6, edge=0x0
[ 0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171015c90f, max_idle_ns: 440795203080 ns
[ 0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns
[ 0.008297] Console: colour dummy device 80x25
[ 0.012550] console [tty0] enabled
[ 0.015915] bootconsole [cdns0] disabled
[ 0.019823] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.99 BogoMIPS (lpj=399996)
[ 0.019836] pid_max: default: 32768 minimum: 301
[ 0.019938] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.019951] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.020537] ASID allocator initialised with 65536 entries
[ 0.020589] Hierarchical SRCU implementation.
[ 0.020911] EFI services will not be available.
[ 0.020937] zynqmp_plat_init Platform Management API v1.0
[ 0.020946] zynqmp_plat_init Trustzone version v1.0
[ 0.021044] smp: Bringing up secondary CPUs ...
[ 0.021290] Detected VIPT I-cache on CPU1
[ 0.021318] CPU1: Booted secondary processor [410fd034]
[ 0.021590] Detected VIPT I-cache on CPU2
[ 0.021608] CPU2: Booted secondary processor [410fd034]
[ 0.021868] Detected VIPT I-cache on CPU3
[ 0.021886] CPU3: Booted secondary processor [410fd034]
[ 0.021926] smp: Brought up 1 node, 4 CPUs
[ 0.021958] SMP: Total of 4 processors activated.
[ 0.021966] CPU features: detected feature: 32-bit EL0 Support
[ 0.021976] CPU: All CPU(s) started at EL2
[ 0.021991] alternatives: patching kernel code
[ 0.022666] devtmpfs: initialized
[ 0.029166] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.029191] futex hash table entries: 1024 (order: 5, 131072 bytes)
[ 0.033992] xor: measuring software checksum speed
[ 0.071907] 8regs : 2303.000 MB/sec
[ 0.111938] 8regs_prefetch: 2053.000 MB/sec
[ 0.151968] 32regs : 2830.000 MB/sec
[ 0.191999] 32regs_prefetch: 2381.000 MB/sec
[ 0.192006] xor: using function: 32regs (2830.000 MB/sec)
[ 0.192077] pinctrl core: initialized pinctrl subsystem
[ 0.192575] NET: Registered protocol family 16
[ 0.193590] vdso: 2 pages (1 code @ ffffff8008ab6000, 1 data @ ffffff8008fc4000)
[ 0.193607] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.194122] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.223457] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed
[ 0.223942] ARM CCI_400_r1 PMU driver probed
[ 0.228028] zynqmp-pinctrl ff180000.pinctrl: zynqmp pinctrl initialized
[ 0.237926] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.304142] raid6: int64x1 gen() 402 MB/s
[ 0.372209] raid6: int64x1 xor() 446 MB/s
[ 0.440253] raid6: int64x2 gen() 688 MB/s
[ 0.508266] raid6: int64x2 xor() 603 MB/s
[ 0.576309] raid6: int64x4 gen() 1042 MB/s
[ 0.644361] raid6: int64x4 xor() 742 MB/s
[ 0.712441] raid6: int64x8 gen() 980 MB/s
[ 0.780446] raid6: int64x8 xor() 745 MB/s
[ 0.848511] raid6: neonx1 gen() 726 MB/s
[ 0.916554] raid6: neonx1 xor() 851 MB/s
[ 0.984628] raid6: neonx2 gen() 1169 MB/s
[ 1.052633] raid6: neonx2 xor() 1208 MB/s
[ 1.120693] raid6: neonx4 gen() 1505 MB/s
[ 1.188747] raid6: neonx4 xor() 1442 MB/s
[ 1.256777] raid6: neonx8 gen() 1651 MB/s
[ 1.324845] raid6: neonx8 xor() 1534 MB/s
[ 1.324853] raid6: using algorithm neonx8 gen() 1651 MB/s
[ 1.324860] raid6: .... xor() 1534 MB/s, rmw enabled
[ 1.324867] raid6: using neon recovery algorithm
[ 1.325790] SCSI subsystem initialized
[ 1.325952] usbcore: registered new interface driver usbfs
[ 1.325990] usbcore: registered new interface driver hub
[ 1.326028] usbcore: registered new device driver usb
[ 1.326087] media: Linux media interface: v0.10
[ 1.326112] Linux video capture interface: v2.00
[ 1.326149] pps_core: LinuxPPS API ver. 1 registered
[ 1.326157] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 1.326176] PTP clock support registered
[ 1.326208] EDAC MC: Ver: 3.0.0
[ 1.326496] zynqmp-ipi ff9905c0.mailbox: Probed ZynqMP IPI Mailbox driver.
[ 1.326665] FPGA manager framework
[ 1.326770] fpga-region fpga-full: FPGA Region probed
[ 1.326878] Advanced Linux Sound Architecture Driver Initialized.
[ 1.327124] Bluetooth: Core ver 2.22
[ 1.327152] NET: Registered protocol family 31
[ 1.327160] Bluetooth: HCI device and connection manager initialized
[ 1.327172] Bluetooth: HCI socket layer initialized
[ 1.327181] Bluetooth: L2CAP socket layer initialized
[ 1.327199] Bluetooth: SCO socket layer initialized
[ 1.327672] clocksource: Switched to clocksource arch_sys_counter
[ 1.327747] VFS: Disk quotas dquot_6.6.0
[ 1.327794] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 1.332510] NET: Registered protocol family 2
[ 1.332795] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[ 1.332907] TCP bind hash table entries: 16384 (order: 6, 262144 bytes)
[ 1.333103] TCP: Hash tables configured (established 16384 bind 16384)
[ 1.333167] UDP hash table entries: 1024 (order: 3, 32768 bytes)
[ 1.333212] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
[ 1.333328] NET: Registered protocol family 1
[ 1.333489] RPC: Registered named UNIX socket transport module.
[ 1.333499] RPC: Registered udp transport module.
[ 1.333506] RPC: Registered tcp transport module.
[ 1.333513] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.333604] Trying to unpack rootfs image as initramfs...
[ 1.919262] Freeing initrd memory: 12480K
[ 1.919700] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[ 1.919862] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 1.920614] audit: initializing netlink subsys (disabled)
[ 1.920697] audit: type=2000 audit(1.908:1): state=initialized audit_enabled=0 res=1
[ 1.921004] workingset: timestamp_bits=62 max_order=19 bucket_order=0
[ 1.921695] NFS: Registering the id_resolver key type
[ 1.921714] Key type id_resolver registered
[ 1.921722] Key type id_legacy registered
[ 1.921734] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 1.921754] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 1.948130] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 1.948150] io scheduler noop registered
[ 1.948158] io scheduler deadline registered
[ 1.948179] io scheduler cfq registered (default)
[ 1.948187] io scheduler mq-deadline registered
[ 1.948194] io scheduler kyber registered
[ 1.948872] nwl-pcie fd0e0000.pcie: Link is DOWN
[ 1.948914] OF: PCI: host bridge /amba/pcie@fd0e0000 ranges:
[ 1.948936] OF: PCI: MEM 0xe0000000..0xefffffff -> 0xe0000000
[ 1.948948] OF: PCI: MEM 0x600000000..0x7ffffffff -> 0x600000000
[ 1.949077] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00
[ 1.949091] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 1.949102] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff]
[ 1.949112] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref]
[ 1.949269] pci 0000:00:00.0: ignoring class 0x068000 (doesn't match header type 01)
[ 1.949854] pci 0000:00:00.0: not setting up bridge for bus 0000:01
[ 1.951408] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
[ 1.951837] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
[ 1.951987] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
[ 1.952133] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
[ 1.952280] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
[ 1.952429] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
[ 1.952580] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
[ 1.952739] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
[ 1.952887] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
[ 1.977904] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[ 1.981631] cacheinfo: Unable to detect cache hierarchy for CPU 0
[ 1.985768] brd: module loaded
[ 1.989060] loop: module loaded
[ 1.989891] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.992161] libphy: Fixed MDIO Bus: probed
[ 1.993141] tun: Universal TUN/TAP device driver, 1.6
[ 1.993284] CAN device driver interface
[ 1.993931] macb ff0b0000.ethernet: Not enabling partial store and forward
[ 1.994373] macb ff0b0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0b0000 irq 23 (00:0a:35:12:34:56)
[ 1.994642] macb ff0e0000.ethernet: Not enabling partial store and forward
[ 1.994975] macb ff0e0000.ethernet eth1: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 24 (00:0a:35:00:22:01)
[ 1.995379] libphy: macb_mii_bus: probed
[ 1.999160] usbcore: registered new interface driver asix
[ 1.999218] usbcore: registered new interface driver ax88179_178a
[ 1.999249] usbcore: registered new interface driver cdc_ether
[ 1.999278] usbcore: registered new interface driver net1080
[ 1.999307] usbcore: registered new interface driver cdc_subset
[ 1.999336] usbcore: registered new interface driver zaurus
[ 1.999375] usbcore: registered new interface driver cdc_ncm
[ 1.999652] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[ 2.000100] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.000111] ehci-pci: EHCI PCI platform driver
[ 2.000433] usbcore: registered new interface driver uas
[ 2.000470] usbcore: registered new interface driver usb-storage
[ 2.000980] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0
[ 2.001049] i2c /dev entries driver
[ 2.001397] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 26
[ 2.001630] IR NEC protocol handler initialized
[ 2.001639] IR RC5(x/sz) protocol handler initialized
[ 2.001646] IR RC6 protocol handler initialized
[ 2.001653] IR JVC protocol handler initialized
[ 2.001659] IR Sony protocol handler initialized
[ 2.001666] IR SANYO protocol handler initialized
[ 2.001673] IR Sharp protocol handler initialized
[ 2.001680] IR MCE Keyboard/mouse protocol handler initialized
[ 2.001687] IR XMP protocol handler initialized
[ 2.002878] usbcore: registered new interface driver uvcvideo
[ 2.002887] USB Video Class driver (1.1.1)
[ 2.003357] Bluetooth: HCI UART driver ver 2.3
[ 2.003368] Bluetooth: HCI UART protocol H4 registered
[ 2.003376] Bluetooth: HCI UART protocol BCSP registered
[ 2.003403] Bluetooth: HCI UART protocol LL registered
[ 2.003411] Bluetooth: HCI UART protocol ATH3K registered
[ 2.003418] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 2.003466] Bluetooth: HCI UART protocol Intel registered
[ 2.003475] Bluetooth: HCI UART protocol QCA registered
[ 2.003511] usbcore: registered new interface driver bcm203x
[ 2.003543] usbcore: registered new interface driver bpa10x
[ 2.003576] usbcore: registered new interface driver bfusb
[ 2.003610] usbcore: registered new interface driver btusb
[ 2.003619] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
[ 2.003715] usbcore: registered new interface driver ath3k
[ 2.004050] EDAC MC0: Giving out device to module 1 controller synps_ddr_controller: DEV synps_edac (INTERRUPT)
[ 2.004243] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
[ 2.004759] CPUidle arm: Failed to register cpuidle driver
[ 2.004926] sdhci: Secure Digital Host Controller Interface driver
[ 2.004935] sdhci: Copyright(c) Pierre Ossman
[ 2.004941] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.047684] mmc0: SDHCI controller on ff160000.sdhci [ff160000.sdhci] using ADMA 64-bit
[ 2.095683] mmc1: SDHCI controller on ff170000.sdhci [ff170000.sdhci] using ADMA 64-bit
[ 2.101706] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.101855] usbcore: registered new interface driver usbhid
[ 2.101864] usbhid: USB HID core driver
[ 2.102738] adrv9009 spi1.0: adrv9009_probe : enter
[ 2.105294] ad9528 spi1.1: spi1.1 supply vcc not found, using dummy regulator
[ 2.118047] mmc0: new HS200 MMC card at address 0001
[ 2.118273] mmcblk0: mmc0:0001 W52516 14.3 GiB
[ 2.118348] mmcblk0boot0: mmc0:0001 W52516 partition 1 4.00 MiB
[ 2.118422] mmcblk0boot1: mmc0:0001 W52516 partition 2 4.00 MiB
[ 2.118490] mmcblk0rpmb: mmc0:0001 W52516 partition 3 4.00 MiB
[ 2.119266] mmcblk0: p1
[ 2.130625] axi_adxcvr a0080000.axi_adxcvr: AXI-ADXCVR-RX (16.01.a) using GTH4 at 0xA0080000 mapped to 0xffffff800cd90000. Number of lanes: 2.
[ 2.131914] axi_adxcvr a0090000.axi_adxcvr: AXI-ADXCVR-RX (16.01.a) using GTH4 at 0xA0090000 mapped to 0xffffff800cfb0000. Number of lanes: 2.
[ 2.132203] axi_adxcvr a00b0000.axi_adxcvr: AXI-ADXCVR-TX (16.01.a) using GTH4 at 0xA00B0000 mapped to 0xffffff800d1d0000. Number of lanes: 4.
[ 2.133760] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[ 2.134600] pktgen: Packet Generator for packet performance testing. Version: 2.75
[ 2.134775] Netfilter messages via NETLINK v0.30.
[ 2.134888] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 2.135024] Initializing XFRM netlink socket
[ 2.135085] NET: Registered protocol family 10
[ 2.135543] Segment Routing with IPv6
[ 2.135588] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 2.135781] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 2.136093] NET: Registered protocol family 17
[ 2.136109] NET: Registered protocol family 15
[ 2.136126] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 2.136140] Ebtables v2.0 registered
[ 2.136221] can: controller area network core (rev 20170425 abi 9)
[ 2.136254] NET: Registered protocol family 29
[ 2.136264] can: raw protocol (rev 20170425)
[ 2.136271] can: broadcast manager protocol (rev 20170425 t)
[ 2.136282] can: netlink gateway (rev 20170425) max_hops=1
[ 2.136478] Bluetooth: RFCOMM TTY layer initialized
[ 2.136489] Bluetooth: RFCOMM socket layer initialized
[ 2.136507] Bluetooth: RFCOMM ver 1.11
[ 2.136517] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.136525] Bluetooth: BNEP filters: protocol multicast
[ 2.136535] Bluetooth: BNEP socket layer initialized
[ 2.136542] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.136552] Bluetooth: HIDP socket layer initialized
[ 2.136667] 9pnet: Installing 9P2000 support
[ 2.136685] Key type dns_resolver registered
[ 2.137041] registered taskstats version 1
[ 2.137364] Btrfs loaded, crc32c=crc32c-generic
[ 2.142645] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 40, base_baud = 6249999) is a xuartps
[ 2.145546] mmc1: new high speed SDHC card at address 59b4
[ 2.145736] mmcblk1: mmc1:59b4 USD 14.7 GiB
[ 2.147832] mmcblk1: p1 p2 p3
[ 3.773859] console [ttyPS0] enabled
[ 3.778647] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:8 protocol:4 pll_locked:yes
[ 3.786792] PLL: shutdown
[ 3.789460] PLL: shutdown
[ 3.792383] PLL: enable
[ 3.794864] PLL: shutdown
[ 3.798214] PLL: enable
[ 3.800678] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
[ 3.811284] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
[ 3.819260] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
[ 3.827500] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[ 3.839860] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[ 3.852431] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed
[ 3.862526] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
[ 3.869397] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.875931] [drm] No driver support for vblank timestamp query.
[ 3.881893] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008b669e8)
[ 4.967687] [drm] Cannot find any crtc or sizes
[ 4.972306] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0
[ 4.980338] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed
[ 4.989162] dwc3-of-simple ff9d0000.usb0: dwc3_simple_set_phydata: Can't find usb3-phy
[ 4.997965] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 5.003384] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 5.011243] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x22010010
[ 5.019886] xhci-hcd xhci-hcd.0.auto: irq 51, io mem 0xfe200000
[ 5.025867] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 5.032577] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 5.039779] usb usb1: Product: xHCI Host Controller
[ 5.044636] usb usb1: Manufacturer: Linux 4.14.0 xhci-hcd
[ 5.050017] usb usb1: SerialNumber: xhci-hcd.0.auto
[ 5.055135] hub 1-0:1.0: USB hub found
[ 5.058824] hub 1-0:1.0: 1 port detected
[ 5.062882] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 5.068299] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 5.075982] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 5.084080] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[ 5.090792] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 5.097995] usb usb2: Product: xHCI Host Controller
[ 5.102853] usb usb2: Manufacturer: Linux 4.14.0 xhci-hcd
[ 5.108234] usb usb2: SerialNumber: xhci-hcd.0.auto
[ 5.113325] hub 2-0:1.0: USB hub found
[ 5.117012] hub 2-0:1.0: 1 port detected
[ 5.121079] dwc3 fe200000.dwc3: couldn't register cable notifier
[ 5.127004] dwc3 fe200000.dwc3: failed to initialize dual-role
[ 5.132839] platform fe200000.dwc3: runtime PM trying to suspend device but active child
[ 5.140892] dwc3: probe of fe200000.dwc3 failed with error -22
[ 5.147133] adrv9009 spi1.0: adrv9009_probe : enter
[ 5.154560] adrv9009 spi1.0: Request deframer lanerate 4096000 kHz failed (-22)
[ 5.161807] adrv9009 spi1.0: Request deframer lanerate 4096000 kHz failed (-22)
[ 5.169100] adrv9009: probe of spi1.0 failed with error -22
[ 5.175935] rtc_zynqmp ffa60000.rtc: setting system clock to 1970-01-01 00:00:10 UTC (10)
[ 5.184037] of_cfs_init
[ 5.186468] of_cfs_init: OK
[ 5.189438] clk: Not disabling unused clocks
[ 5.193669] ALSA device list:
[ 5.196578] #0: DisplayPort monitor
[ 5.200640] Freeing unused kernel memory: 512K
INIT: version 2.88 booting
Starting udev
[ 5.309540] udevd[1830]: starting version 3.2.2
[ 5.318654] udevd[1831]: starting eudev-3.2.2
[ 5.378523] zynqmp_r5_remoteproc ff9a0100.zynqmp_r5_rproc: RPU core_conf: split0
[ 5.386356] remoteproc remoteproc0: ff9a0100.zynqmp_r5_rproc is available
[ 5.393246] zynqmp_r5_remoteproc ff9a0200.zynqmp_r5_rproc: RPU core_conf: split1
[ 5.400904] remoteproc remoteproc1: ff9a0200.zynqmp_r5_rproc is available
[ 5.864239] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 5.974778] EXT4-fs (mmcblk1p3): recovery complete
[ 5.979516] EXT4-fs (mmcblk1p3): mounted filesystem with ordered data mode. Opts: (null)
[ 5.987691] EXT4-fs (mmcblk1p2): recovery complete
[ 5.992423] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
Tue Feb 9 11:33:24 UTC 2021
[ 6.235716] [drm] Cannot find any crtc or sizes
Starting internet superserver: inetd.
Configuring packages on first boot....
(This may take several minutes. Please do not power off the machine.)
Running postinst /etc/rpm-postinsts/100-sysvinit-inittab...
update-rc.d: /etc/init.d/run-postinsts exists during rc.d purge (continuing)
INIT: Entering runlevel: 5
Configuring network interfaces... [ 6.496846] Micrel KSZ9031 Gigabit PHY ff0e0000.mdio-mii:03: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=ff0e0000.mdio-mii:03, irq=POLL)
[ 6.512616] pps pps0: new PPS source ptp0
[ 6.516559] macb ff0b0000.ethernet: gem-ptp-timer ptp clock registered.
[ 6.523208] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
udhcpc (v1.24.1) started
Sending discover...
[ 9.579978] macb ff0b0000.ethernet eth0: link up (1000/Full)
[ 9.585579] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Sending discover...
[ 11.627920] macb ff0b0000.ethernet eth0: link down
Sending discover...
No lease, forking to background
[ 15.780846] Micrel KSZ9031 Gigabit PHY ff0e0000.mdio-mii:07: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=ff0e0000.mdio-mii:07, irq=POLL)
[ 15.796380] pps pps1: new PPS source ptp1
[ 15.800326] macb ff0e0000.ethernet: gem-ptp-timer ptp clock registered.
[ 15.806970] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
udhcpc (v1.24.1) started
Sending discover...
[ 17.771989] macb ff0b0000.ethernet eth0: link up (1000/Full)
Sending discover...
Sending discover...
No lease, forking to background
done.
Starting system message bus: dbus.
Starting Dropbear SSH server: Generating key, this may take a while...
Public key portion is:
ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAABAQCI/LI5UX4ktYmI1Qt49sdgdRh8uK2nys84aVJjfCX9lHl2VwbPXslJxnNEvq256JYMdZThFUgZ7HDK6mj2NlHwpNbc+1nfC1K8WFDRYW0aAbK6EOFzcoz9liOtwEY44cI0LJEsilsO9noXHxiK+jLpqhQyH/6sIEA7LJmwOwRM4zQT7+B73vmA8pnabLKFSgbVL+4MyQdKH9aYWuBtBUge9+ZUrqpgD1wK4nY0Ws0QaNq0COrHaQ11Xxx3jdA7aGLxkXoOyCg+eN39Er2DV55198F4CVziJj44Y1wHPnTRSUSTZwzLkCuHpf6MqYIIjhaXPG9hfvIp3NcUEXwBfoSb root@frm127101u1r1
Fingerprint: md5 59:9e:aa:7a:2a:4a:23:d4:03:88:ec:c4:d9:bc:9c:08
dropbear.
Starting syslogd/klogd: done
Starting tcf-agent: OK
PetaLinux 2018.2 frm127101u1r1 /dev/ttyPS0
frm127101u1r1 login: