Post Go back to editing

Does ADRV9008 DC offset calibration suitable in 5G with subcarrier at DC

Thread Summary

The user inquires about the impact of DC offset calibration on 5G signals with subcarriers at DC in the ADRV9008. The final answer indicates that RF DC offset does not affect the useful signal, but digital DC offset can impact peak EVM for subcarriers at DC. The user can disable digital DC offset calibration using the API adi_adrv9025_DigDcOffsetEnableSet() and adjust the M-shift value to check performance. The RF DC offset calibration mask bit D3 in ug1295 refers to RF DC offset calibration.
AI Generated Content

Hi expert,

As I known from ug1295 the ADRV9008 hardware reference manul, DC calibration include RF and digital DC offset calibration. But I don't know exactely the procedure of the calibration, like if the radio is off during init calibration and tracking calibration. The reason why I want to know that is I want to know if the DC offset calibration is suitable in 5G with subcarrier at DC. Should I disable this DC offset calibration function or disable during tracking calibration.

Thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.