ADRV9026
Recommended for New Designs
The ADRV9026 is a highly integrated, radio frequency (RF) agile transceiver offering four independently controlled transmitters, dedicated observation...
Datasheet
ADRV9026 on Analog.com
Hi,
According to ug-1727 there is a "Pattern Generator" and written"There is also a way the user can load a custom pattern into the framer which can be verified on the baseband processor"
So, How can I set the pattern and run test data?
I'm using ADRV9026
Thanx!
__CommunityServer__Service__ - Moved from TES GUI & Software support ADRV9009/ADRV9008-1/ADRV9008-2 to Design Support ADRV9008-1/ADRV9008-2/ADRV9009. Post date updated from Sunday, June 14, 2020 5:53 AM UTC to Thursday, January 22, 2026 7:26 PM UTC to reflect the move.
If you are testing on EVB and TES GUI setup, please use the attached iron python script to load custom patterns.
After executing the script, capture the RX data and check whether the transmitted and receive patterns are matching.
Thank for your response!
But we are not running with ADI's GUI, instead we use Xilinx FPGA and "ADRV9026 Released Software Package SW2.0.0.16"
In your script you set "FrmTestDataCfg=Types.adi_adrv9010_FrmTestDataCfg_t()" And i cant find:
1. "Types" field in "adi_adrv9025_FrmTestDataCfg" structure
2. "adi_adrv9010_FrmTestDataCfg_t" function doesn't exists
Please refer to adi_adrv9025_FramerTestDataSet API from adi_adrv9025_data_interface.h file.
**
* \brief Selects the PRBS type and enables or disables RX Framer PRBS generation
*
* This is a debug function to be used for debug of the Rx JESD204B lanes.
* Rx data transmission on the JESD204B link(s) is not possible
* when the framer test data is activated. To disable PRBS call this function
* again with the framer data source set to FTD_ADC_DATA.
*
* \pre This function may be called any time after device initialization
*
* \dep_begin
* \dep{device->common.devHalInfo}
* \dep_end
*
* \param device is a pointer to the device settings structure
* \param frmTestDataCfg is a pointer to a structure which contains the framer(s) of interest, testDataSource and injectPoint
*
*\retval ADI_COMMON_ACT_WARN_RESET_LOG Recovery action for log reset
* \retval ADI_COMMON_ACT_ERR_CHECK_PARAM Recovery action for bad parameter check
* \retval ADI_ADRV9025_ACT_ERR_RESET_SPI Recovery action for SPI reset required
* \retval ADI_COMMON_ACT_NO_ACTION Function completed successfully, no action required
*/
int32_t adi_adrv9025_FramerTestDataSet(adi_adrv9025_Device_t *device,
adi_adrv9025_FrmTestDataCfg_t *frmTestDataCfg);
Please refer to adi_adrv9025_FrmTestDataCfg_t from adi_adrv9025_data_interface_types.h file.
/**
* \brief Data structure to hold ADRV9025 JESD204b Framer Test data and debug configuration
*/
typedef struct adi_adrv9025_FrmTestDataCfg
{
uint8_t framerSelMask;
adi_adrv9025_FramerDataSource_e testDataSource;
adi_adrv9025_FramerDataInjectPoint_e injectPoint;
} adi_adrv9025_FrmTestDataCfg_t;
Thank for effort!
Its exactly my problem, according to quoted by you code section, how can I set the field Type= "my custom pattern" ? "Type" field is not part of "adi_adrv9025_FrmTestDataCfg_t" structure
In your python script you used with a statement "FrmTestDataCfg = Types.adi_adrv9010_FrmTestDataCfg_t()" , and what's the equivalent to this in "ADRV9026 Released Software Package SW2.0.0.16"
my code is:
adi_adrv9025_FrmTestDataCfg_t frmTestDataCfg;
<here I should set my custom pattern>
frmTestDataCfg.framerSelMask = ADI_ADRV9025_FRAMER_0;
frmTestDataCfg.testDataSource = ADI_ADRV9025_FTD_PATTERN_REPEAT;
frmTestDataCfg.injectPoint = ADI_ADRV9025_FTD_SERIALIZER;
<here I should set my custom pattern>
The custom pattern is set through the SPIWrites.
##### YOUR CODE GOES HERE #####
#set the 16 bit user pattern
#Test data to transmitted
spiWrite(0x6e32, 0x55)
spiWrite(0x6e33, 0x55)
In your python script you used with a statement "FrmTestDataCfg = Types.adi_adrv9010_FrmTestDataCfg_t()" , and what's the equivalent to this in "ADRV9026 Released Software Package SW2.0.0.16"
Please refer to the example code available in main.c file inside the API package. (Adi.Adrv9025.CustomerPkg_broad_market.2.0.0.12\Adi.Adrv9025.Api\src_broad_market\c_src\app\example.main.c)
You need to use something similar below for adi_adrv9025_FramerTestDataSet API.
/* Setup internal Tx test tone frequency */
adi_adrv9025_TxTestToneCfg_t toneCfg = { 0 };
toneCfg.txChannelMask = ADI_ADRV9025_TXALL;
toneCfg.txToneFreq_Hz = 500000;
toneCfg.txToneGain = ADI_ADRV9025_TX_NCO_0_DB;
toneCfg.enable = 1;
recoveryAction = adi_adrv9025_TxTestToneSet(adrv9025Device, &toneCfg, 1);
if (recoveryAction != ADI_COMMON_ACT_NO_ACTION)
{
printf("Failed to setup ADRV9025 Tx Test Tone\n");
printf("ERROR: Error number %d, Recovery action %d. In file %s, in function %s, in line %d, variable name %s. Error message %s.\n",
adrv9025Device->common.error.errCode,
adrv9025Device->common.error.newAction,
adrv9025Device->common.error.errFile,
adrv9025Device->common.error.errFunc,
adrv9025Device->common.error.errLine,
adrv9025Device->common.error.varName,
adrv9025Device->common.error.errormessage);
/* Call action handler */
return ADI_COMMON_ACT_ERR_RESET_FULL;
}
Thanks a lot for your detailed help!
Hi,
About the
#set the 16 bit user pattern
#Test data to transmitted
spiWrite(0x6e32, 0x55)
spiWrite(0x6e33, 0x55)
The limit of pattern is only 16bits? Can we set a pattern of 64bit or larger?
You can have only a 16-bit value.
Thanx,
Do we can set different test pattern of 16bits for each lane?
It is not possible to set different test pattern for each lane simultaneously.
The same data will be transmitted on all enabled lanes.