Post Go back to editing

ERROR: 294: TALISE_waitArmCmdStatus() failed due to thrown ARM error. Is device in correct state for calling command?

Hallo all, 

I am trying to create a new soft instead using IIO Oscilloscope based on ADRV9009+zcu102. Currently, I have a  data in the input of the adrv9009 chip which comes from my BBG( i already test it and it works)

that I had created before, 

but when I run  my program I have these 2 errors there in the window below 

I tried also  to ignore the calibration but it caused other problems for example radio on 

should i change something in your code ,or do something else?

I have the impression that it could not pass from state to another.

I'm really lost.

take look please below when i skipped   the calibration 

just for information
I kept the same program (configuration) in app_talise.c

Thank you

OPokoy