Is the reference clock of ADRV9009 from the clock generator (DCLK of AD9528 or any other JESD clock generator) should be in the value of 122.88, 184.32 or 245.76?(from the table 41 of UG-1295)
Aren't we allowed to generate any other frequencies which would be the even integer multiple of SYSREF( DCLK = 2N*SYSREF)?
The SYSREF is dependent on Fs which in turn dependent on the baseband signal's characteristics.
Edit Notes
provided the reference from user guide[edited by: s.kannan at 10:55 AM (GMT 0) on 4 May 2020]