Post Go back to editing

ADRV9009 RF-SOM multichip sync

Thread Summary

The user inquires about synchronizing two ADRV9009 transceivers with one HMC7044 clock generator, specifically regarding the sysref signal mode and synchronization issues. The final answer recommends using a single-shot sysref for JESD bring-up and RF phase synchronization, emphasizing that the sysref should reach both ADRV9009 and FPGA simultaneously to avoid phase discrepancies. The accompanying answers clarify that continuous sysref can cause issues due to skew and that a central sysref distribution is necessary for simultaneous MCS sequences, especially when using separate deframers for each ADRV9009.
AI Generated Content

Hello,

In RF-SOM clock tree, I see 1 HMC7044  generate ref_clk and sys_ref for 2 ADRV9009. I have some questions:

1. How to synchronize 2 ADRV9009 with 1 HMC7044, sysref signal is 1 shot or continuous? (I have synchronized 2 adrv9009 eval board with 1 shot sysref and continuous-sysref is not ok)

2. Can I synchronize number of HMC7044 in 1-pulse mode? I try but it doesn't work.

3. 8 ADRV9009's phase difference is const every times power up or after boot, we have to calibrate again.

Thanks.

Parents Reply Children
No Data