KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
ADRV9009
Recommended for New Designs
The ADRV9009 is a highly integrated, radio frequency (RF), agile transceiver offering dual transmitters and receivers, integrated synthesizers, and digital...
Datasheet
ADRV9009 on Analog.com
HMC7044
Not Recommended for New Designs
The HMC7044 is a high performance, dual-loop, integer-N jitter attenuator capable of performing reference selection and generation of ultralow phase noise...
Datasheet
HMC7044 on Analog.com
AD9528
Recommended for New Designs
The AD9528 is a two-stage PLL with an integrated JESD204B/JESD204C SYSREF generator for multiple device synchronization. The first stage phase-locked loop...
Datasheet
AD9528 on Analog.com
Hello,
I try to synchronize 2 ADRV9009 boards. I use Kintex Ultrascale FPGA and HMC7044 EVA board to generate reference clock and sysref signal. AD9528's outputs to ADRV9009/FPGA are distributed from VCXO, sysref signals to ADRV9009/FPGA are from external.
I see in Multichip Sync section of User Guide that two ADRV9009's device clocks and sysref signals are from only 1 AD9528. Is my structure possible? I connect 1 TX to 4 RX, 2 RX signals in TX's board is stable, other RX are not stable. Please give me some advice.
Thanks.

Can you please check the MCS status?
Hope you have enabled the RF Phase Sync option. Are you seeing phase variation boot to boot?
Can you please share more details on the measurements?.
I use mode RF phase sync init and continuous tracking. Mcs status is ok (Reg value is 0x0B).
Ref clocks for ADRV are from AD9528's VCXO, they are synchronised. I enable sysref signal after both ADRVs have been enable MCS mode.
I set Baker 13 code in TX. After divider, RF signal goes to 2 RX in 2 different boards. RX signal in the board, which does not have TX, is not stable. LO frequency is 3GHz. I wonder the LOs in 2 boards are not synchronized.
I check mcs status is 0x0b, so CLKPLL SDM is not sync.
Adrv9009 has 3 PLLs, they are synchronized at the same time, aren't they?
In my case, I connect 1 TX to 1 RX in same board and 1 RX in other board. Ref_clk is 245.76MHz,
+ LO 3GHz: 2 RX phases in 2 board are not same in different power up time.
+ LO 2,94912GHz: 2 RX phases are same in different power up time.
I try the case: ref_clk and sys_ref of 2 adrv9009 are from 1 ad9528. Outputs are synchronized at LO frequency = N* ref_clk with N is integer and not synchronized with N is fractional.
What is the API version you are using?
Arm version is 6.0.2. I use newest no-os library and modify it to fit with my project.
Can you please confirm what is the API version?
https://github.com/analogdevicesinc/no-OS/tree/master/drivers/rf-transceiver/talise
Thank you,
API version is 3.6.0.5.
Ref_clk signals are synchronised. Sys_ref signals come to ADRVs at same time, continuous and phases are constanst.
Mcs status is 0x0b.
Sync mode is init and conTrack.
Procedure after power up:
- ad9528 initialize (off sysRef)
- adrv initialize
- getPllsLockStatus
- enableMultichipSync(1,&mcsstatus)
- on sysref
- enableMultichipSync(0,&mcsstatus)
- initArm
- loadStreamFromBinary
- loadArmFromBinary
- verifyArmCheckSum
- setRfPllFrequency
- getPllsLockstatus
- runInitCals
- waitInitCals
- config jesd204
- enableTrackingCals
- radioOn
- enable TX and RX
What can I do to solve the problem?
+ LO 3GHz: 2 RX phases in 2 board are not same in different power up time
What is the relative phase difference you are measuring from boot to boot?
How is the Tx phase synchronization between the two ADRV9009?
RX phase difference is random value.
I haven't measured TX phase. I think if RF PLLs are synchronized, both TX and RX are synchronized. Is it true?
I haven't measured TX phase. I think if RF PLLs are synchronized, both TX and RX are synchronized. Is it true?
Yes , same LO is used for Tx and Rx and RF phase sync adjust the Sigma delta modulator phase to have same phase as Ref_CLK.
How are you measuring Rx phase from 2 different ADRV9009 boards. ?
If Tx is phase synced then Rx should also maintain same phase.
Have you tried enabling tracking cal as well. ? ( TAL_RFPLLMCS_INIT_AND_CONTTRACK = 3)
I connect 1 TX to 2 RX by a divider. The RX data is sent from 1 FPGA to the other by MGT transceivers. Compare 2 signal, I calculate the different phase.
I have tried enable TAL_RFPLLMCS_INIT_AND_CONTTRACK and other sync mode, but the same results.
I connect 1 TX to 2 RX by a divider. The RX data is sent from 1 FPGA to the other by MGT transceivers. Compare 2 signal, I calculate the different phase.
I have tried enable TAL_RFPLLMCS_INIT_AND_CONTTRACK and other sync mode, but the same results.