Post Go back to editing

adrv9009 multichip sync

Thread Summary

The user is trying to synchronize two ADRV9009 boards using a Kintex Ultrascale FPGA and HMC7044 EVA board for reference clock and SYSREF signals. Despite the MCS status being 0x0B and the reference clocks being synchronized, the RX phases on the two boards are inconsistent when using a fractional LO frequency (3 GHz) but consistent with an integer LO frequency (2.94912 GHz). The final advice is to ensure the device clocks and SYSREF signals reach both ADRV9009 boards simultaneously and to check the phase variation across frequency, which can be corrected in baseband.
AI Generated Content

Hello,

I try to synchronize 2 ADRV9009 boards. I use Kintex Ultrascale FPGA and HMC7044 EVA board to generate reference clock and sysref signal. AD9528's outputs to ADRV9009/FPGA are distributed from VCXO, sysref signals to ADRV9009/FPGA are from external.

I see in Multichip Sync section of User Guide that two ADRV9009's device clocks and sysref signals are from only 1 AD9528. Is my structure possible? I connect 1 TX to 4 RX, 2 RX signals in TX's board is stable, other RX are not stable. Please give me some advice.

Thanks.

Parents Reply
  • Adrv9009 has 3 PLLs, they are synchronized at the same time, aren't they? 

     In my case, I  connect 1 TX to 1 RX in same board and 1 RX in other board. Ref_clk is 245.76MHz,

    + LO 3GHz: 2 RX phases in 2 board are not same in different power up time.

    + LO 2,94912GHz: 2 RX phases are same in different power up time.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.