KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADRV9009
Recommended for New Designs
The ADRV9009 is a highly integrated, radio frequency (RF), agile transceiver offering dual transmitters and receivers, integrated synthesizers, and digital...
Datasheet
ADRV9009 on Analog.com
HMC7044
Not Recommended for New Designs
The HMC7044 is a high performance, dual-loop, integer-N jitter attenuator capable of performing reference selection and generation of ultralow phase noise...
Datasheet
HMC7044 on Analog.com
AD9528
Recommended for New Designs
The AD9528 is a two-stage PLL with an integrated JESD204B/JESD204C SYSREF generator for multiple device synchronization. The first stage phase-locked loop...
Datasheet
AD9528 on Analog.com
Hello,
I try to synchronize 2 ADRV9009 boards. I use Kintex Ultrascale FPGA and HMC7044 EVA board to generate reference clock and sysref signal. AD9528's outputs to ADRV9009/FPGA are distributed from VCXO, sysref signals to ADRV9009/FPGA are from external.
I see in Multichip Sync section of User Guide that two ADRV9009's device clocks and sysref signals are from only 1 AD9528. Is my structure possible? I connect 1 TX to 4 RX, 2 RX signals in TX's board is stable, other RX are not stable. Please give me some advice.
Thanks.

Can you please check the MCS status?
Hope you have enabled the RF Phase Sync option. Are you seeing phase variation boot to boot?
Can you please share more details on the measurements?.
I use mode RF phase sync init and continuous tracking. Mcs status is ok (Reg value is 0x0B).
Ref clocks for ADRV are from AD9528's VCXO, they are synchronised. I enable sysref signal after both ADRVs have been enable MCS mode.
I set Baker 13 code in TX. After divider, RF signal goes to 2 RX in 2 different boards. RX signal in the board, which does not have TX, is not stable. LO frequency is 3GHz. I wonder the LOs in 2 boards are not synchronized.
I use mode RF phase sync init and continuous tracking. Mcs status is ok (Reg value is 0x0B).
Ref clocks for ADRV are from AD9528's VCXO, they are synchronised. I enable sysref signal after both ADRVs have been enable MCS mode.
I set Baker 13 code in TX. After divider, RF signal goes to 2 RX in 2 different boards. RX signal in the board, which does not have TX, is not stable. LO frequency is 3GHz. I wonder the LOs in 2 boards are not synchronized.
We have provision in ADRV9009 evaluation board to share Sysref and Dev clock to second board. Please refer this post, https://ez.analog.com/wide-band-rf-transceivers/design-support-adrv9008-1-adrv9008-2-adrv9009/f/q-a/105981/two-adrv9009-eval-boards-on-zcu102
In your case there are three PLL-VCO circuits, there will be some phase mismatch over time because of 3 different VCO's. (the drift with time and temp may not be same for all 3). So It is recommended to try above mentioned option.
One thing you can try is to make sure that Dev clk reaching both ADRV9009 and FPGA are at same time. You can adjust delays available with AD9528 and HMC chip for that. Still not sure what accuracy you will get from this setup.
I try the case: ref_clk and sys_ref of 2 adrv9009 are from 1 ad9528. Outputs are synchronized at LO frequency = N* ref_clk with N is integer and not synchronized with N is fractional.
Am I wrong somewhere?
If you have enabled RF phase sync option , it should work.
when you say
not synchronized with N is fractional.
RF phase is not synchronised for LO frequency using fractional words? what offset are you seeing between and integer frequency and next fractional frequency?
I check mcs status is 0x0b, so CLKPLL SDM is not sync.
Adrv9009 has 3 PLLs, they are synchronized at the same time, aren't they?
In my case, I connect 1 TX to 1 RX in same board and 1 RX in other board. Ref_clk is 245.76MHz,
+ LO 3GHz: 2 RX phases in 2 board are not same in different power up time.
+ LO 2,94912GHz: 2 RX phases are same in different power up time.
I try the case: ref_clk and sys_ref of 2 adrv9009 are from 1 ad9528. Outputs are synchronized at LO frequency = N* ref_clk with N is integer and not synchronized with N is fractional.
What is the API version you are using?
Arm version is 6.0.2. I use newest no-os library and modify it to fit with my project.
Can you please confirm what is the API version?
https://github.com/analogdevicesinc/no-OS/tree/master/drivers/rf-transceiver/talise
Thank you,
API version is 3.6.0.5.
Ref_clk signals are synchronised. Sys_ref signals come to ADRVs at same time, continuous and phases are constanst.
Mcs status is 0x0b.
Sync mode is init and conTrack.
Procedure after power up:
- ad9528 initialize (off sysRef)
- adrv initialize
- getPllsLockStatus
- enableMultichipSync(1,&mcsstatus)
- on sysref
- enableMultichipSync(0,&mcsstatus)
- initArm
- loadStreamFromBinary
- loadArmFromBinary
- verifyArmCheckSum
- setRfPllFrequency
- getPllsLockstatus
- runInitCals
- waitInitCals
- config jesd204
- enableTrackingCals
- radioOn
- enable TX and RX
What can I do to solve the problem?
+ LO 3GHz: 2 RX phases in 2 board are not same in different power up time
What is the relative phase difference you are measuring from boot to boot?
How is the Tx phase synchronization between the two ADRV9009?