Post Go back to editing

ZC706 + ADRV9009 Linux image SD card - boot crash

Thread Summary

The user attempted to run TES (Transceiver Evaluation Software) for the ADRV9009 on a ZC706 board, but the board crashes after displaying the Linux Penguin. TES is only supported on the ZYNQ3 platform, not the ZC706, due to SERDES speed limitations. The user should use the ZYNQ3 board for TES, as documented in the ADRV9009 evaluation user guide and product page.
AI Generated Content

Hello,

I have a ZC706 board from Xilinx and I want to run TES for the ADRV9009.

I found this link and downloaded the zipped folder

https://www.analog.com/media/en/evaluation-boards-kits/evaluation-software/ADRV9009-SDCARD.zip

Under Windows 10 I copied all the contents to a 8GB SD card and install it on the ZC706.

The ZC706 boot and crash just after displaying the Linux Penguin.

What I make wrong ?

Thanks Panou

Thread Notes

Parents Reply Children
  • OK I understand better now. This something also very still strange for me . Inside the ADRV9009-SDCARD.zip there is a folder update_ZC706 which content uImage and device.dtb from 2016 ! How can be possible to have files that are from 2016 and others from 2018 ? 

    So to work with ADRV9009 you need 1600USD(ADRV9009)+3300USD(ZYNQ3)+2500USD(ZCU102) = 7400USD to do the same that was possible to do with the ADRV9371 and ZC706 ... nice ... 

    Panou

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.