Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Support ADRV9001 – ADRV9007
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Support ADRV9001 – ADRV9007
  • RF & Microwave
  • RF Transceivers
  • Support ADRV9001 – ADRV9007
  • Cancel
Support ADRV9001 – ADRV9007
Documents Analog and Half-Band Peak Detectors
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +Debug: FAQ
  • -Device Configurations: FAQ
    • Analog and Half-Band Peak Detectors
    • +Automated TDD
    • +Digital Pre-Distortion
    • Implement an External LNA in TES
  • +Physical Design of Customer Systems: FAQ
  • +Produce Sample Code
  • +Quick Start: FAQ
  • +SD Card Image: FAQ
  • +SDK Errata: FAQ
  • +Software Functions: FAQ

Analog and Half-Band Peak Detectors

Introduction

This section describes how a signal is processed by a Transimpedance Amplifier (TIA)  , Analog-to-Digital Converter (ADC), and Half-Band filter (HB), and how this affects the triggering of analog and HB peak detectors.  

     

Figure 1. ADRV9001 Rx Chain

      Figure 2. ADRV9001 Rx Chain and Frequency Response 

Figures 1 and 2 illustrate the receiving (Rx) chain of a system. Figure 1 provides a block diagram overview, while Figure 2 details the signal's journey through key components showcasing the working of peak detectors. As shown in Figure 2, the input signal, at a frequency equal to the Radio Frequency (RF) carrier plus the Intermediate Frequency (IF), is first processed by an analog mixer. This mixer shifts the signal down to the IF by combining it with a Local Oscillator (LO) signal matching the RF carrier. The resulting IF signal is then passed through the TIA, converting it from a current to a voltage suitable for the ADC. One must note that the TIA frequency response is like that of an LPF, which also attenuates signals outside the band of interes t. Then this signal is passed through the LPF which further attenuates the out-of-band signals. The user can configure the LPF within TES as shown in Figure 3.

Figure 3. LPF Configuration 

The ADRV9002 offers selectable LPF orders:

  • First-order: Reduces power consumption but provides lower image rejection.
  • Second-order: Improves image rejection but increases power consumption.

Figure 4 illustrates the frequency response of both first and second-order LPFs. This information is also available in the user guide. The LPF primarily serves to prevent aliasing and is not intended as a substitute for external signal filtering.

Figure 4. RX LPF Frequency Response at Different f1db Configuration

Before the ADC an Analog Peak Detector (APD) is placed for monitoring the peak power of the signal entering the ADC. Here the APD monitors the signal peak power; once the signal is above the certain threshold value provided by the user, this results in a flag in the gain control block. Then ADC digitizes the signal for further processing. This digitized signal is passed through the Half-Band (HB) filter and at this stage the HB peak detector monitors the signal, which may again result in a flag in the gain control block. The gain control block (see Figure 1) uses a combination of the APD upper threshold and the HB peak detector upper threshold to decide the level by which the attenuation will be adjusted in the front-end attenuator block. The peak detector configuration can be done in TES as shown in Figure 5. ADRV9002 has the flexibility to control the external gain block as well.

Figure 5. Peak Detector Configuration

The HB filtering is determined by the system clock rate ((± 25*(System Clock))/184.32 MHz) and the system clock rate is depended on the profile. The frequency response of the filter is not given in the user guide. Instead, it is provided in a separate file: hb1.mat. The Figure 6 shows the filter magnitude response of HB filter for system clock of 150 MHz, 184.32 MHz and 200 MHz.

Figure 6. HB Filter Magnitude Response

Steps for Obtaining the HB Filter response using hb1.mat

  • Load the file using the MATLAB Command: load('hb1.mat').
  • We will see a set of data as shown in Figure 7.

Figure 7. hb1.mat Data

  • The filter coefficients are stored in decflt_h.
  • Now use the function fvtool(decflt_h) to get the filter response. The filter response looks as shown in Figure 8.

Figure 8. Normalized Frequency Filter Magnitude Response

  • In the filter visualization tool, we see two options: one is analysis parameters and the other is sampling frequency as shown in Figure 9.



     Figure 9. Filter Visualization Tool Options

  • In the Analysis parameters, we can change the plot axis as shown below. In this case, the normalize frequency option will be unchecked

Figure 10. Analysis Parameter

  • Once the above parameters are set, click on sampling frequency option and change the sampling frequency (Fs) to the system clock frequency (in this case, 184.32 MHz). The passband frequency is 25 MHz.

  Figure 11. System Clock Rate

  • The below figure shows the filter response

Figure 12. Filter Magnitude Response for System Clock Rate of 184.32 MHz

Please find the hb1.mat file.

hb1.zip 

Tags: ADRV9002 Wideband Transceiver IC RF Integrated Transceivers
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • HMC441LP3 has no nominal broadband gain over the frequency range
    Liuccc
    Hi, I made an amplifier using HMC441LP3. However, over the frequency range from 6.5 GHz to 13.5 GHz, the circuit doesn't work as it is specified in the datasheet of the chip. From 6 GHz to 10 GHz, the...
  • RE: ADRV9002 Central Frequency offset and noisy spectrum
    Ruairí
    Hi Evgeny, Narrow band (NB) on this part works in a low IF mode, there is some filtering on the input and we do not tune the desired signal to the zero IF because the LO noise will affect the signal...
  • CMOS prescaler turns the ADALM1000 into MHz Frequency meter
    dmercer
    Virtual Classroom for ADI University Program - The idea is very simple and commonly used. Just divide the high frequency signal with a prescaler down to frequencies low enough to measure with the ALM1000. Then the measured frequency is multiplied by...
 
Related Content
  • HMC441LP3 has no nominal broadband gain over the frequency range
    Liuccc
    Hi, I made an amplifier using HMC441LP3. However, over the frequency range from 6.5 GHz to 13.5 GHz, the circuit doesn't work as it is specified in the datasheet of the chip. From 6 GHz to 10 GHz, the...
  • RE: ADRV9002 Central Frequency offset and noisy spectrum
    Ruairí
    Hi Evgeny, Narrow band (NB) on this part works in a low IF mode, there is some filtering on the input and we do not tune the desired signal to the zero IF because the LO noise will affect the signal...
  • CMOS prescaler turns the ADALM1000 into MHz Frequency meter
    dmercer
    Virtual Classroom for ADI University Program - The idea is very simple and commonly used. Just divide the high frequency signal with a prescaler down to frequencies low enough to measure with the ALM1000. Then the measured frequency is multiplied by...