Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
Support ADRV9001 – ADRV9007
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Support ADRV9001 – ADRV9007
  • RF & Microwave
  • RF Transceivers
  • Support ADRV9001 – ADRV9007
  • Cancel
Support ADRV9001 – ADRV9007
Documents 3) Transmit/Receive Example
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +Debug: FAQ
  • +Device Configurations: FAQ
  • +Physical Design of Customer Systems: FAQ
  • +Produce Sample Code
  • -Quick Start: FAQ
    • 1) Installation and Configuration
    • 2) Connection to TES
    • 3) Transmit/Receive Example
  • +SD Card Image: FAQ
  • +SDK Errata: FAQ
  • +Software Functions: FAQ

3) Transmit/Receive Example

In this section, a simple transmit and receive configuration will be set up and observed.

1) Start by connecting a signal generator to the port labelled "RX1A_IN" and connecting a spectrum analyzer to the port labelled "TX1_OUT".

2) In the "Device Configuration" sub tab under the "Configure" tab, we will set up a narrowband configuration. The device can be set to "TDD" and "DMR". The traffic light system will tell you if your configuration is valid. Default setting can be kept for the rest of the page.

3) Next, in the "Carriers" sub tab, set the Rx1 carrier frequency to 700MHz (the intermediate frequency can remain at the default 490 kHz). Set the Tx1 carrier frequency to 1600 MHz. The rest of the settings on this page can remain as default.

4) You can now view the Rx/Tx overview tabs to see if you are satisfied.

5) To program the part click the "Program" button. Ensure that signal generator output is not turned on during programming.

Once programmed, you will see "Programmed" on the screen as shown.

6) In the transmit tab, along the left side you will see a "Data Source" dropdown menu. Select "Single Tone" from the menu. Click the play icon when you are ready. 

In this example, the tone is placed 3 kHz from the carrier.

You should now also be able to see this tone on the connected spectrum analyzer.

Press the stop button before the next step.

7) Now, we will view the Receive tab.

Set your signal generator to 700.002 MHz and amplitude of -10 dBm. Turn on the output of your signal generator.

You should now be able to see a tone at the set frequency.

If the tone is not exactly where it is expected, try using an external LO from the "Carriers" sub tab in the "Configure" tab.

8) When shutting down the system, ensure to go to File > Shut Down Platform to safely shut down.

For more detailed information please refer to the ADRV9001 Evaluation System section of the user guide.

Tags: tes transmit tx Transceiver Evaluation Software ADRV9002 ADRV9001 rx receive Show More
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • Configuration #0
    ADIApproved
    We’ll begin by considering one of the simplest configurations. This configuration is also detailed from another perspective on YouTube Step 1: Configure the device Let’s begin by configuring the...
  • RE: ADAU1761 DAC & ADC setting
    DaveThib
    Hello jjin, This part is very difficult to visualize what the signal flow is by only using the register names and listing. With SigmaStudio you can see the signal flow easily and setup the part the...
  • FDD Repeater / RF Converter Setup
    ConradCollins
    ADRV9001 has internal loopbacks that can be used in a FDD repeater / RF converter application. This guide will demonstrate how to set this up in TES. 1) Set up the device to your desired configuration...
 
Related Content
  • Configuration #0
    ADIApproved
    We’ll begin by considering one of the simplest configurations. This configuration is also detailed from another perspective on YouTube Step 1: Configure the device Let’s begin by configuring the...
  • RE: ADAU1761 DAC & ADC setting
    DaveThib
    Hello jjin, This part is very difficult to visualize what the signal flow is by only using the register names and listing. With SigmaStudio you can see the signal flow easily and setup the part the...
  • FDD Repeater / RF Converter Setup
    ConradCollins
    ADRV9001 has internal loopbacks that can be used in a FDD repeater / RF converter application. This guide will demonstrate how to set this up in TES. 1) Set up the device to your desired configuration...