Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Support ADRV9001 – ADRV9007
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Support ADRV9001 – ADRV9007
  • RF & Microwave
  • RF Transceivers
  • Support ADRV9001 – ADRV9007
  • Cancel
Support ADRV9001 – ADRV9007
Documents SD Card Image: FAQ
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +Debug: FAQ
  • +Device Configurations: FAQ
  • +Physical Design of Customer Systems: FAQ
  • +Produce Sample Code
  • +Quick Start: FAQ
  • -SD Card Image: FAQ
    • a) Writing SD Card Image Manually (SDK23.1 and Higher)
    • b) SD Card image using ADRV9001 Disk Imaging Utility (SDK 13 or higher)
    • c) SD Card image using ADRV9001 Disk Imaging Utility (Legacy - SDK 12 or lower)
  • +SDK Errata: FAQ
  • +Software Functions: FAQ

SD Card Image: FAQ

In this tab we will show a step-by-step guide to image or re-image SD the FPGA SD card for releases up to version 12 and for version 13 and beyond. 

These guides can be used to create a new SD card or fix a corrupted SD card.

As a guide for knowing whether you are using Pre-Release Silicon (B0) vs. Released Silicon (C0), here's a list of the Evaluation Board and SD card labels for each revision*:

B0

C0

SD Card Label:
(Only works with B0 Silicon)


SD Card Label:
(Works with B0 or C0 Silicon)


Evaluation Board Label:

W1:

W2:

Evaluation Board Label:

W1:

W2:

*The safest way to check this is by connecting to TES and viewing the Silicon version

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • New working standard SD card image for TES.
    gverma
    1) My TES Standard SD card is corrupted? Where to download new working image? 2) I am having issue with TES connection to zynq with current standard SD card. Where do I get a working image?
  • RE: The SD card need image. Is this contents in SD card right? In the second picture.
    ADIApproved
    Yes this is the image you need to download and write it in SD card.
  • RE: Need SD card replacement??
    fanchenjuan@163.com
    I need a sd card of ad9371, I download the latest image to sd card but cannot work correct
 
Related Content
  • New working standard SD card image for TES.
    gverma
    1) My TES Standard SD card is corrupted? Where to download new working image? 2) I am having issue with TES connection to zynq with current standard SD card. Where do I get a working image?
  • RE: The SD card need image. Is this contents in SD card right? In the second picture.
    ADIApproved
    Yes this is the image you need to download and write it in SD card.
  • RE: Need SD card replacement??
    fanchenjuan@163.com
    I need a sd card of ad9371, I download the latest image to sd card but cannot work correct