Post Go back to editing

ADRV9002 Model in ADISimRF

Thread Summary

The user asked if the ADRV9002 RX model in ADIsimRF includes the effects of the balun, representing performance at a 50 Ω interface. The final answer confirms that the ADRV9002 model in ADIsimRF uses a 50 Ω impedance for performance simulations, validating the user's assumption.
AI Generated Content
Category: Hardware
Product Number: ADRV9002

According to the ADRV9002 datasheet, all performance and parameter graphs include the effects of the baluns required in the RX and TX paths to match a 50 Ω system impedance to the device's 100 Ω differential port impedance.

Based on this, can we assume that the ADRV9002 RX model available in ADISimRF also includes the effects of the balun, and therefore already represents the performance at the 50 Ω interface? Is this assumption correct?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.