Hello, I am working with the ADRV9002 ZCU102 reference design and I would like to use the transceiver with RX1, RX2, and TX1 enabled while completely disabling TX2. To do this, I enabled the Disable Tx2 SSI option in the axi_adrv9001 IP configuration and removed the TX2-related blocks from the Vivado Block Design, including util_dac_2_upack, axi_adrv9001_tx2_dma, and all associated TX2 AXI-Stream connections, clocks, resets, and external ports. I then regenerated the HDL wrapper, updated system_top.v to remove all TX2-related ports and connections, and updated the XDC constraints to remove TX2 differential I/O ports and constraints. I also rebuilt the Yocto EDF Linux image and updated the Device Tree by removing the TX2 DMAC node, the TX2 AXI core node, the TX2 TDD node, TX2 GPIO references, and TX2-related frequency-hopping settings. The modified bitstream is generated successfully and Linux boots correctly. The ADRV9002 is detected on SPI and bound to the expected driver. However, no ADRV9002-related IIO devices are created; only the Xilinx AMS IIO device is visible under /sys/bus/iio/devices The kernel reports the following errors:
[ 3.520157] cf_axi_adc 84a00000.axi-adrv9002-rx-lpc: probe with driver cf_axi_adc failed with error -22
[ 20.459065] platform 84a09000.axi-adrv9002-rx2-lpc: deferred probe pending: (reason unknown)
[ 20.459072] platform 84a0c800.axi-adrv9002-core-tdd1-lpc: deferred probe pending: (reason unknown)
[ 20.459079] platform 84a0a000.axi-adrv9002-tx-lpc: deferred probe pending: (reason unknown)
Could you please confirm whether a 2RX/1TX configuration with TX2 SSI disabled is supported by the axi_adrv9001 HDL IP and the Linux IIO drivers? Is removing util_dac_2_upack and axi_adrv9001_tx2_dma the correct procedure after enabling Disable Tx2 SSI, or are further HDL, Device Tree, or driver changes required? Could the cf_axi_adc probe failure with error -22 indicate an unsupported configuration or an HDL/Linux driver version mismatch?
Thank you for your help.