Post Go back to editing

Inquiry about TDD enableSetupDelay, FDD workaround, and LO sharing

Thread Summary

The user inquired about configuring the ADRV9002 for TDD mode with an enableSetupDelay less than 8us, which is not possible. A workaround is to use FDD mode and externally control TX and RX signals to simulate TDD, while sharing the same LO across all channels. For fast-switching requirements, the user is advised to explore alternative ADI transceiver products.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADRV9002

Hello,

I am currently working with the ADRV9002 and have a few questions regarding the TDD mode timing configuration, external control, and LO setup.

  1. Is there any way to configure the enableSetupDelay to be less than 8us in TDD mode? If so, could you please provide guidance on how to achieve this?

  2. If reducing the delay below 8us is not possible in TDD mode, would it be a valid workaround to configure the device in FDD mode and externally control the TX and RX signals to simulate TDD operation? (Note: For our application, both TX and RX will use the exact same frequency).

  3. In this setup, is it possible to share the same Local Oscillator (LO) across all channels (TX1, TX2, RX1, and RX2)?

  4. Are there any other technical considerations, limitations, or potential issues we should be aware of when attempting this configuration?

  5. If using the ADRV9002 with the FDD workaround is not feasible for our fast-switching requirements, are there any other alternative ADI transceiver products you would recommend?

Thank you for your support.

Parents
  • Hello Vanitha,

    Thank you for your response. I have a few follow-up questions:

    1. LO Sharing Configuration in FDD Mode: When configured to FDD mode, the Local configuration options become disabled. Is there a specific method or workaround to configure the Local Oscillator (LO) so that it is shared across all channels (Tx1, Tx2, Rx1, and Rx2) in FDD mode?

    Thank you for your support!

Reply
  • Hello Vanitha,

    Thank you for your response. I have a few follow-up questions:

    1. LO Sharing Configuration in FDD Mode: When configured to FDD mode, the Local configuration options become disabled. Is there a specific method or workaround to configure the Local Oscillator (LO) so that it is shared across all channels (Tx1, Tx2, Rx1, and Rx2) in FDD mode?

    Thank you for your support!

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.