Post Go back to editing

Frequency hopping in ADRV 9005 via SPI mode

Category: Software
Product Number: ADRV9005

Hi Team,

we are working on ADRV9005 configuration Generated the C99 code from TES and integrated with custom MCU.

we have generated the custom TDD profile with 25KHz BW 192kHz sample rate TX LO 80MHz.

Enabled the internal tone and we can be able see the LO on TX LO 0f 80MHz in Defined carrier frequency mode.

Next, we have implemented the FH support into our application by generating the C99 from TES. But this is not working we can't see any LO on the TX.

we need to support via SPI mode for hopping instead of GPIO.

Followed the following order:

error_code = initialize(adrv9001Device_0);
if (0 != error_code) { return error_code; }

error_code = calibrate(adrv9001Device_0);
if (0 != error_code) { return error_code; }

error_code = configure(adrv9001Device_0);
if (0 != error_code) { return error_code; }

error_code = prime(adrv9001Device_0);
if (0 != error_code) { return error_code; }

error_code = beginReceiving(adrv9001Device_0);
if (0 != error_code) { return error_code; }

error_code = beginTransmitting(adrv9001Device_0);
if (0 != error_code) { return error_code; }

while(1)

{

error_code = adi_adrv9001_fh_Hop(adrv9001Device_0, ADI_ADRV9001_FH_HOP_SIGNAL_1);
ADI_HANDLE_ERROR(error_code, adrv9001Device_0);

customer_TimerWait_us(NULL, 5000);

error_code = adi_adrv9001_Radio_Channel_EnableRf(adrv9001Device_0, ADI_TX, ADI_CHANNEL_1, true);
ADI_HANDLE_ERROR(error_code, adrv9001Device_0);

}

 

we have verified the adi_adrv9001_fh_Configuration_Inspect and adi_adrv9001_fh_HopTable_Inspect these things looks fine, but still the TX LO is missing. 

Same internal tone is also used in the FH case as like DCF mode.

Are there any order of Api's to hop the signal.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.