Hello community!
In our application, we utilize LO1 for Rx1 and Rx2 with, e.g., NCO 15 MHz, and LO2 for Tx2 on a single ADRV9002.
I am interested in a frequency error when Rx1 and Rx2 receives transmitted Tx2 signal on the same frequency. So, LO1 is set to (f_carrier-NCO) and LO2 is set to f_carrier. We tested that in the range of f_carrier between 300 to 450 MHz, it is usually below 1 Hz.
Based on Device Clock, NCO frequency, Sample Rate and possibly further parameters, is it possible to characterize this error between LO1 and LO2 when assigned the same frequencies?
NCO frequency can be modified in our application (it could be variable above 5 MHz value). Can you provide a way/strategy to zeroize this LO1 - LO2 frequency error?
If not, could you describe the frequency error by a formula?
If not, would you expect this frequency error to be periodic, with respect to carrier frequency?

Many thanks!
Jakub