Post Go back to editing

How to get TES working on custom board (Bytepipe)

Thread Summary

The user asked if custom boards can connect to TES over Ethernet, and it was confirmed that custom boards cannot connect to TES. The TES GUI does not support byte pipe platforms, and for more details, the user should contact the byte pipe company with the inbuilt ADRV9002. The FPGA in use is the Zynq Ultrascale+ MPSOC (3cg).
AI Generated Content
Category: Software
Product Number: ADRV9002
Software Version: v29

Online search results have provided that custom boards cannot connect to TES over ethernet. Is this true?

If it is true, do dev kits like the zcu102 have special hardware or software installed to enable a live TES connection?

The FPGA I'm using is the Zynq Ultrascale+ MPSOC (3cg).