For the ADRV9003, the customer is going to operate in SPI mode. For this mode, the user's guide specifies that certain pins, such as RX1_EN and RX2_EN should not be connected. However, the customer has a design that uses these signals to enable other devices (LNAs). If the device is in SPI mode and a RX1_EN is asserted, will the ADRV9003 ignore this signal, will it be confused, or will it cause damage? I suspect that the device being in SPI mode will ignore the pin assertions and it seems unlikely that this would cause any damage, but I would like to confirm this. Thanks!