Post Go back to editing

TES Connection Error with ADRV9001 + ZC706/ZCU102 Insufficient Disk Space

Thread Summary

The user encountered an 'Insufficient Disk Space' error when trying to connect and run TES/SDK29 on both ZC706 and ZCU102 platforms. The final solution involved manually partitioning the Linux partition as per the provided document, which resolved the issue on the ZC706. The user will attempt the same solution on the ZCU102.
AI Generated Content
Category: Software
Product Number: ADRV9002
Software Version: TES & SDK 0.29

I am unable to connect and run TES/SDK29.  TES/SDK24 runs okay.  I tried it on both ZC706 and ZCU102 platform.

I've programmed the SD cards per the instructions on the web. I tried 16GB and 32GB cards and different computers.

I connect with a USB/LAN dongle, IPV4 set to 192.168.1.2. 

I can ping 192.168.1.10 and can connect and log in with PuTTY.

I get the following error when I try to connect with TES:

Session log file
Created on Monday, February 23, 2026 at 22:50:05.5719053, Greenwich Mean Time.

-------------------------------------------------------------------

Processing command-line arguments:

Booting up Argo 0.29.0.2025 from C:\Program Files\Analog Devices\ADRV9001 Transceiver Evaluation Software.

Processing command-line arguments:

Temp files will be stored in C:\Users\hardware-shared\AppData\Local\Temp\Analog Devices\Argo.

User files will be stored in C:\Users\hardware-shared\AppData\Roaming\Analog Devices\Argo.

Attempting to initialize Windows Forms elements.

Located user settings file at C:\Users\hardware-shared\AppData\Roaming\Analog Devices\Argo\Navassa.Periplous.json.

Located default config file for plugin at C:\Program Files\Analog Devices\ADRV9001 Transceiver Evaluation Software\Navassa.Periplous.taxidi.

Located user settings file at C:\Users\hardware-shared\AppData\Roaming\Analog Devices\Argo\Navassa.Periplous.json.

Creating load-save object with file C:\Program Files\Analog Devices\ADRV9001 Transceiver Evaluation Software\Navassa.Periplous.taxidi.

Loading plugin Navassa v0.29.0.

Connection attempt initiated.

Last resource version sync was v0.24.0

Cleaning platform resources directory.

Performing platform resource sync.


Insufficient Disk Space
The remote host was online, but the necessary files could not be copied. This usually happens when the Linux partition has insufficient free disk space. Consider deleting unneeded files, or try the 'Expand Partition' action under the 'File' menu.

Preparing to kill any existing server(s).

Preparing to kill server.

Host: root@192.168.1.10, Server: Adrv9001Server* located in /home/analog/adrv9001_server/resources/Adi.Adrv9001.Server/

Preparing to start server.

Host: root@192.168.1.10, Server: Adrv9001Server_C0 located in /home/analog/adrv9001_server/resources/Adi.Adrv9001.Server/

System.IO.FileNotFoundException: No files found matching base filename Adrv9001Server_C0
at AnalogDevices.EvalClient.DirectoryDescriptor.GetLatestFileVersion(String fileNameWithoutVersion)
at AnalogDevices.EvalClient.SshServerManager.StartAndLog(String args, String logFileNameOnly)
at AnalogDevices.Argo.Models.ConnectionModel.StartServer() in C:\Jenkins\workspace\_github_navassa-installer_master\navassa-periplous\argo\Argo.Navis\Argo.Navis\Models\ConnectionModel.cs:line 400
at AnalogDevices.Argo.Models.ConnectionModel.connect_DoWork(Object data) in C:\Jenkins\workspace\_github_navassa-installer_master\navassa-periplous\argo\Argo.Navis\Argo.Navis\Models\ConnectionModel.cs:line 472

Parents Reply Children
No Data