>> 1 ADRV9005 can support Tx tracking cals when configured for TDD profiles. Not available during FDD operation.
Can the ADRV9005 be used in continuous TX mode (100% duty cycle) with DPD enabled if we do not use the receiver?
Specifically, can the device operate permanently in TX while using the RX path as ORX for DPD feedback, without requiring any RX - TX state transitions?
For context, we’re considering this because the 1T2R versions do not support DPD, and the ADRV9002 option is "significantly" more expensive.