Post Go back to editing

ADRV9005 - Continuous TX (100% duty) with DPD

Thread Summary

The user asks if the ADRV9005 can operate in continuous TX mode (100% duty cycle) with DPD enabled, using the RX path as ORX for DPD feedback without RX-TX state transitions. The final answer confirms that this is possible. The ADRV9005 supports DPD in TDD profiles, but not in FDD operation.
AI Generated Content
Category: Hardware
Product Number: ADRV9005

>> 1 ADRV9005 can support Tx tracking cals when configured for TDD profiles. Not available during FDD operation.


Can the ADRV9005 be used in continuous TX mode (100% duty cycle) with DPD enabled if we do not use the receiver?
Specifically, can the device operate permanently in TX while using the RX path as ORX for DPD feedback, without requiring any RX - TX state transitions?

For context, we’re considering this because the 1T2R versions do not support DPD, and the ADRV9002 option is "significantly" more expensive.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.