Hello,
I have a ADRV9002NP/W1/PCBZ board connected to a ZCU102 board.
With the latest master no-OS branch clone built software (DMA_DEMO) executes as expected there is not any TX output signal.
Xilinx Zynq MP First Stage Boot Loader
Release 2022.2 Feb 11 2026 - 05:16:02
PMU-FW is not running, certain applications may not be supported.
Hello
ADRV9002 Rev 12.0, Firmware 0.22.39, Stream 0.7.15.0, API version: 68.14.13 successfully initialized
axi-adrv9002-rx-lpc: Successfully initialized (122888183 Hz)
axi-adrv9002-tx-lpc: Successfully initialized (122888183 Hz)
axi-adrv9002-rx2-lpc: Successfully initialized (122888183 Hz)
axi-adrv9002-tx2-lpc: Successfully initialized (122894287 Hz)
DMA_EXAMPLE Rx2: address=0x163400 samples=32768 channels=2 bits=16
DMA_EXAMPLE Rx1: address=0x153400 samples=32768 channels=2 bits=16
Bye
Thanks,
Ilya