Hopefully an easy one for the Experts to answer...
Table 14 in the datasheet states that the RF Ports will handle 25 dBm CW for >7 years if the Front End attenuator is set to 30 dB. (Assumes device is powered)
However, page 270 of ug1828 states that the "maximum safe input power is 18 dBm (peak)" for the Rx ports. Its unclear if this limit assumes any FE attenuation or if the device is even powered or not.
In our application, the preceding RF chain includes gain such that weak signals of interest occupy >-60 dBFS. To monitor stronger signals we can introduce 30 dB of attenuation. However, when the attenuation is not enabled, unexpected blockers may exceed 0 dBFS. Although not ideal, we can accept blockers exceeding the dynamic range but we must also ensure that they do not cause damage.
For reliable operation, should we limit input power at the ADRV9002 pin to below +18 dBm or are we OK follow datasheet Table 14?