Post Go back to editing

AGC Threshold Level

Thread Summary

The user inquired about AGC parameters, specifically if the ADP threshold levels of -27 dBFS (overload) and -30 dBFS (underload) are too low, causing the Rx Gain Index to stick at its minimum. The final answer advised increasing the gap between thresholds to -15 dBFS (overload) and -40 dBFS (underload) to improve detection reliability and avoid the stuck gain issue. Additionally, setting `lowThreshPreventGainInc = false` is recommended to allow gain increases with low input levels. A known issue with the AGC was mentioned, and the user was directed to a relevant thread for more details.
AI Generated Content
Category: Hardware
Product Number: ADRV9002

Dear Specialists,

I have a question regarding the AGC parameters.
Regarding the ADP threshold levels, are the following values too low?

Peak Overload Threshold = -27 dBFS
Peak Underload Threshold = -30 dBFS

When there is no RF input, the Rx Gain Index sticks at its minimum.
I want to keep the LSSI output amplitude relatively low, so I'm trying to activate the AGC with a lower RF input level.
Could you offer any advice?

Regards,

Parents Reply Children