Post Go back to editing

AGC Threshold Level

Thread Summary

The user inquired about AGC parameters, specifically if the ADP threshold levels of -27 dBFS (overload) and -30 dBFS (underload) are too low, causing the Rx Gain Index to stick at its minimum. The final answer advised increasing the gap between thresholds to -15 dBFS (overload) and -40 dBFS (underload) to improve detection reliability and avoid the stuck gain issue. Additionally, setting `lowThreshPreventGainInc = false` is recommended to allow gain increases with low input levels. A known issue with the AGC was mentioned, and the user was directed to a relevant thread for more details.
AI Generated Content
Category: Hardware
Product Number: ADRV9002

Dear Specialists,

I have a question regarding the AGC parameters.
Regarding the ADP threshold levels, are the following values too low?

Peak Overload Threshold = -27 dBFS
Peak Underload Threshold = -30 dBFS

When there is no RF input, the Rx Gain Index sticks at its minimum.
I want to keep the LSSI output amplitude relatively low, so I'm trying to activate the AGC with a lower RF input level.
Could you offer any advice?

Regards,

Parents
  • HI  

    The selected thresholds of –27 dBFS (overload) and –30 dBFS (underload) are indeed quite close together. The AGC’s Peak Detector logic struggles with such narrow margins, especially since it relies on consistent peak measurements. Increase the gap between thresholds to improve detection reliability—e.g., –15 dBFS (overload) and –40 dBFS (underload). This gives the AGC more dynamic range for decision-making and avoids the “stuck at minimum gain” issue.

    Setting lowThreshPreventGainInc = false is essential to allow gain increases when input is low.

    Regards,

    SJ

Reply
  • HI  

    The selected thresholds of –27 dBFS (overload) and –30 dBFS (underload) are indeed quite close together. The AGC’s Peak Detector logic struggles with such narrow margins, especially since it relies on consistent peak measurements. Increase the gap between thresholds to improve detection reliability—e.g., –15 dBFS (overload) and –40 dBFS (underload). This gives the AGC more dynamic range for decision-making and avoids the “stuck at minimum gain” issue.

    Setting lowThreshPreventGainInc = false is essential to allow gain increases when input is low.

    Regards,

    SJ

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.