ADRV9002
Recommended for New Designs
The ADRV9002 is a highly integrated RF transceiver that has dual-channel transmitters, dual-channel receivers, integrated synthesizers, and digital signal...
Datasheet
ADRV9002 on Analog.com
The data shhet show the power sequency for ADRV9002.But The EVK DO NOT follow up it?
From EVK schematic,R812=57.6K,The turn-on delay
CH1=20.8*3=62.4ms connect to VDDA_1P0
CH2=0ms connect to VDDA_1P3
CH3=20.8*6=124.8ms connect to VDDA_1P8
It is not mate with VDDA_1P0 after enabling VDDA_1P3 and VDDA_1P8
Can you explain?
Dorant - Moved from RF and Microwave to Design Support ADRV9001 – ADRV9007. Post date updated from Monday, March 17, 2025 2:04 AM UTC to Monday, March 17, 2025 12:46 PM UTC to reflect the move.
Dorant - Moved from RF and Microwave to Design Support ADRV9001 – ADRV9007. Post date updated from Monday, March 17, 2025 12:46 PM UTC to Monday, March 17, 2025 12:46 PM UTC to reflect the move.
Hi,
As per the ADP5056 datasheet, the sequence is channel 2, channel 1 and channel 3
and if you see the schematic, the power sequence is 1V,1.3V and 1.8V which is mentioned in the datasheet.
Regards
Rahul
Channel 2 is connected to VDIG_1P0.
ADP5056_1P0V is connected to VDIG_1P0 not VDDA_1P0
What is different VDDA_1P0 and VDIG_1P0?
Which (VDDA_1P0 and VDIG_1P0) need to turn on firt?
This is in the user guide, pg308
I am confuse.
Channel 2 : ADP5056_1P0 connected to VDIG_1P0
Channel 1 : ADP5056_1P3 connected to VDDA_1P0
Therefore, VDDA_1P0 power up after VDIG_1P0
But data sheet show VDDA_1P0 should be turn on first.
Where does it state the VDDA_1P0 must power up first? I searched datasheet and user guide.
Channel 2 connected to ADP5056_1P0 and VDIG_1P0
Channel 1 connected to ADP5056_1P3 and VDDA_1P0
Channel 3 connected to ADP5056_1P8
Therefore, Power sequency VDIG_1P0 ,VDDA_1P0,VDDA_1P8
It is violation follow statement
Channel 2 connected to ADP5056_1P0 and VDIG_1P0
Channel 1 connected to ADP5056_1P3 and VDDA_1P0
Channel 3 connected to ADP5056_1P8
Therefore, Power sequency VDIG_1P0 ,VDDA_1P0,VDDA_1P8
It is violation follow statement
Who can answer it?