Post Go back to editing

ADRV9002 Power sequency

Category: Datasheet/Specs
Product Number: ADRV9002

The data shhet show the power sequency for ADRV9002.But The EVK DO NOT follow up it?

From EVK schematic,R812=57.6K,The turn-on delay 

CH1=20.8*3=62.4ms connect to VDDA_1P0

CH2=0ms connect to VDDA_1P3

CH3=20.8*6=124.8ms connect to VDDA_1P8

It is not mate with VDDA_1P0 after enabling VDDA_1P3 and VDDA_1P8

Can you explain?



Update
[edited by: RaySun at 1:44 AM (GMT -4) on 18 Mar 2025]

Thread Notes