Post Go back to editing

Simultaneous transmission and reception

Category: Datasheet/Specs
Product Number: adrv9003

Will there be any issues if i try to transmit and receive at the same frequency at the same time?

Edit Notes

.
[edited by: rahulpillai at 6:14 AM (GMT -5) on 27 Jan 2025]
Parents
  • Hi,

    I have successfully tested simultaneous signal transmission and reception in FDD mode, and it works as expected. However, we do not recommend using the same frequency for both transmission (Tx) and reception (Rx) in FDD mode due to potential interference between the Tx and Rx signals. For example:

    1. Overpowering the Received Signal: Transmitted signals are typically much stronger than incoming signals. Using the same frequency for Tx and Rx can overwhelm the receiver, effectively drowning out incoming signals and preventing proper reception.

    2. Duplexer Limitations: Duplexers, which are designed to isolate transmit and receive signals, cannot achieve perfect isolation on the same frequency. Some transmitted signal may leak into the receiver, leading to interference and degraded performance.

    Regards

    Rahul 

Reply
  • Hi,

    I have successfully tested simultaneous signal transmission and reception in FDD mode, and it works as expected. However, we do not recommend using the same frequency for both transmission (Tx) and reception (Rx) in FDD mode due to potential interference between the Tx and Rx signals. For example:

    1. Overpowering the Received Signal: Transmitted signals are typically much stronger than incoming signals. Using the same frequency for Tx and Rx can overwhelm the receiver, effectively drowning out incoming signals and preventing proper reception.

    2. Duplexer Limitations: Duplexers, which are designed to isolate transmit and receive signals, cannot achieve perfect isolation on the same frequency. Some transmitted signal may leak into the receiver, leading to interference and degraded performance.

    Regards

    Rahul 

Children