Hi. I have an application that requires deterministic latency between Tx and Rx channels of ADRV9002. I know that I need to do multichip synchronization to achieve this. My question is that why is there non-deterministic delay and phase even without MCS on the same ADRV9002 chip even though the source clock is same for both ADC and DAC. Shouldn't the phase and delay of Tx RX channels be sync even without the need of MCS??
Thanks