Hello all,
adi_adrv9001_cals_InitCals_Run()
int32_t adi_adrv9001_cals_InitCals_Run | ( | adi_adrv9001_Device_t * | adrv9001, |
adi_adrv9001_InitCals_t * | initCals, | ||
uint32_t | timeout_ms, | ||
uint8_t * | errorFlag | ||
) |
the above api I've been using for my project, everytime the errorflag is returning as 0 but sometimes one in 1000 its returning the error number "7" in the document "
-
[out] errorFlag A 3-bit error flag that helps identify any errors during Initial calibrations. '0' indicates that there was no error.