Post Go back to editing

RF Bandwidth and Sample Rate in TES

Thread Summary

The user asked about configuring TES for a 20 MHz OFDM signal with a 20 MSPS complex I/Q sample rate. The final answer confirmed that the sample rate in TES should be 4/3 of the RF bandwidth, which explains why 20 MSPS was not accepted. The accompanying answer clarified that for complex signals, the minimum I/Q sample rate is equal to the channel bandwidth, but TES requires a higher sample rate.
AI Generated Content
Category: Software
Product Number: ADRV9002
Software Version: TES 0.25.1

Hello,

Our PHY uses an OFDM signal of 20 MHz (from -10 MHz to 10 MHz) and works with a sample rate of 20 MSPS (complex I/Q samples). I've tried to set up a matching profile with TES, but the latter indicates that the configuration is invalid when I set the Dataport Sample Rate to 20 MSPS and the RF Channel Bandwidth to 20 MHz in the Device Configuration tab for the Rx1/Rx2 parts:

My questions are:

  1. Should the RF Channel Bandwidth be set to the full signal bandwidth (from the lowest negative frequency to the highest positive frequency) or only the positive frequencies part (10 MHz in my case)?
  2. If the answer to the previous question is the full bandwidth, why using a complex sampling rate equal to the RF bandwidth is not enough? Is there a formula that gives the minimum Navassa sampling rate for a specific RF bandwidth?

Thanks.

Edit Notes

Typo
[edited by: Cito at 8:02 PM (GMT -4) on 31 Jul 2024]

Thread Notes

Parents Reply Children
  • Thanks for your answer Rahul.

    However, the minimum sampling rate criterion from the Nyquist–Shannon theorem is a bit different when applied to complex signals: the I and Q components are 2 different samples, so if the sample rate of each component is equal to the channel bandwidth, the full sample rate is twice the channel bandwidth. Thus, the minimum I/Q sample rates for a 20 MHz RF bandwidth is 20 MSPS (per component).

    Or do you mean the sample rate field in TES is actually the full sample rate instead of the per-component sample rate?

    From my tests, it looks like that the minimum sample rate that TES accepts it 4/3 of the RF bandwidth. Is it expected?

    Thanks,
    Cito

  • Hi Cito,

    The sample rate provided in TES will have 4/3 of the RF bandwidth. 

    Regards

    Rahul  

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.