KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
ADRV9002
Recommended for New Designs
The ADRV9002 is a highly integrated RF transceiver that has dual-channel transmitters, dual-channel receivers, integrated synthesizers, and digital signal...
Datasheet
ADRV9002 on Analog.com
Hi everyone,
I have a question on adrv9002
I want to align RX1 and RX2 of one transciver, but I didn't make any connection on MCS port.
however, in user guide (ug1828)
MCS is needed when an application requires deterministic latency among datapaths within one ADRV9001 device or multiple ADRV9001 devices.
Even though it is a single transciver, Is input from external MCS signal absolutely necessary for alignment?
Is there any way to replace it with software?
Sincery,
JaeKyung.
__CommunityServer__Service__ - Moved from TES GUI & Software Support ADRV9001 – ADRV9007 to Design Support ADRV9001 – ADRV9007. Post date updated from Thursday, June 13, 2024 6:53 AM UTC to Thursday, January 22, 2026 11:01 PM UTC to reflect the move.
Hi JaeKyung,
Yes, MCS signal is needed for having the deterministic latency even though it is within a single transceiver (Please refer to MULTICHIP SYNCHRONIZATION chapter in user guide). One to be noted that MCS also provides phase synch capability. For enabling MCS while operating in TES or using the sample code obtain from TES doesn’t required any additional clock source since it takes in 6 pulses required for MCS operation from the FPGA (Xilinx ZC706, Xilinx ZCU102). Nevertheless, external clock source can be used for providing the required pulses.
Regards
Rahul