The datasheet shows some black out zone for the reference clock, however, when I use Navassa eval board, I can inject external device clock frequencies in the middle of these black-out zones, such as 25.6MHz, 38.4MHz and the device is working good.
May I know what is limited by these dead zone? And when I use a external device clock in the middle of these dead zones, the transceiver is working in a reliable status or marginal status? Will there be noticeable degradation if there are power voltage change or ambient temperature change?
P