Post Go back to editing

External LNA with AGC

Thread Summary

The user inquired about achieving 59dB attenuation with two LNAs (30dB each) in their setup, noting the AGC's 30dB limit. The support engineer confirmed that this functionality is available in SDK/TES 0.25.0, suggesting an update. The user reported issues with the gain table indices and external control fields, but the engineer requested the SDK version for further assistance.
AI Generated Content
Category: Hardware
Product Number: ADRV9003

Hello,

I have two LNA in my setup, with 60dB total gain (each has 30dB fixed gain).
According to the AGC, the basic gain table can achieve at most 30dB attenuation.

1. Is there any configuration that I can do to use the 59dB possible attenuation?
2. What is the correct method to define the gain table and how?

Regards,
Yoel

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.