Post Go back to editing

Power error in FDD for Frequency hoppoing

Category: Software
Product Number: ADRV9002
Software Version: NO-OS2021R2

Because I can't generate a FDD hopping profile using TES. So I try to modify the profile that has been generated. I noticed an error in my power configuration API after I changed it. The error content is as follows

[ERROR]: Error number  1 (0x00000001), Recovery action -2.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure_Validate, in line  39, variable name readPattern.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
[ERROR]: Error number  1 (0x00000001), Recovery action -2.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure, in line  70, variable name NULL.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
adrv9002_power_mgmt_config, 614: failed with "ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board" (1)

I didn't have any of these problems with  only Tx in TDD, and I want to know if I modified the parameters correctly, or which parameters I ignored to modify.

The main changes I made from launch only to double hop are
one:
  \"rx1LoSelect\": 1, \
   \"rx2LoSelect\": 1, \
    \"tx1LoSelect\": 1, \
    \"tx2LoSelect\": 1, \
to
    \"rx1LoSelect\": 1, \
    \"rx2LoSelect\": 2, \
    \"tx1LoSelect\": 1, \
    \"tx2LoSelect\": 2, \
two:
    \"duplexMode\": 0, \
to
    \"duplexMode\": 1, \
this is my profile . Can you check for me ?

Edit Notes

IN TDD
[edited by: JS1998 at 12:23 AM (GMT -4) on 14 Mar 2024]

Thread Notes